Strange Neighbourg table

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Strange Neighbourg table

Jump to solution
2,169 Views
zigbee1
Contributor III

We are currently maintaining a  Zigbee controller out of JN5169.
We are using the JN-SW-4170 SDK.
We have of course a good understanding of JN-AN-1216
Application Note: JN-AN-1216 ZigBee 3.0 IoT Control Bridge,

I'm using the LQI Management  Request ( APP_eZdpMgmtLqiRequest()  ) to query the neighbourg table of the Controler as well as the Routers.

I'm currently seen very strange behvaiour at the Controler side

 

Here after is an output of the Neighbourg query of the controller, which I don't understand !! How can the controler 0000 and an othet Router can be Sibling !!!

Node Node Relation Type Deepth LQI Rx-Idle
0000 56fb Child End Device 1 203 Rx-Off
0000 f8d7 Child End Device 1 154 Rx-Off
0000 50e0 Child Router 1 161 Rx-On
0000 cd45 Sibling Router 0 84 Rx-On
0000 5cbe Sibling Router 0 87 Rx-On
0000 ad66 Sibling Router 0 120 Rx-On
0000 50ad Sibling Router 0 77 Rx-On
0000 129a Sibling Router 0 84 Rx-On
0000 cdd5 Sibling Router 0 111 Rx-On

 

 

Labels (2)
Tags (1)
0 Kudos
Reply
1 Solution
2,100 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

I hope you are doing great.

It is ok that the coordinator and the router could be Sibling, because in the Zigbee network the coordinator is a router but it is the one that it has the Trust Center, in this case. 

Regards,

Mario

View solution in original post

0 Kudos
Reply
8 Replies
2,153 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @zigbee1,

I hope you are doing great.

I am not sure if I am following your question. 

What is the command that you are sending? the APP_eZdpMgmtLqiRequest, but what is the device that you are sending this command? to the coordinator? router?

Do you have the terminal logs and the sniffer log for this issue?

Regards,

Mario

0 Kudos
Reply
2,142 Views
zigbee1
Contributor III

Hello Mario,

 

hope you are doing well to.

yes indeed this is based on

case (E_SL_MSG_MANAGEMENT_LQI_REQUEST):
{
uint8 u8StartIndex;
u16TargetAddress = ZNC_RTN_U16 ( au8LinkRxBuffer, 0 );
u8StartIndex = au8LinkRxBuffer[2];
u8Status = APP_eZdpMgmtLqiRequest ( u16TargetAddress
u8StartIndex,
&u8SeqNum );
}

this occurred already by just queering the controller Neighbour table as you can see in the initial post,

 

NO I don't have any sniff as anyhow it won't help since the query is just asking for the Neighbour table of the Zigbee controler

 

The code is coming from the JN-AN-1216-ZigBee-3-0-IoT-ControlBridge

 

 

All code is based with the "ZigbeeNodeControlBridge"

0 Kudos
Reply
2,101 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

I hope you are doing great.

It is ok that the coordinator and the router could be Sibling, because in the Zigbee network the coordinator is a router but it is the one that it has the Trust Center, in this case. 

Regards,

Mario

0 Kudos
Reply
2,096 Views
zigbee1
Contributor III

Hi Mario hope you are doing well.

 

Glad to see that is possible, however this doesn't help me in my drawing of a topology report.
As if a Controller and a or several routers are Sibling, what does that mean from a relationship standpoint ?

I'm quiet lost here , would appreciate NXP insight

0 Kudos
Reply
2,089 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @zigbee1,

As you know the Zigbee protocol is based on the 802.15.4 Specification.

Please look at the next user guide https://www.nxp.com/docs/en/user-guide/JN-UG-3024.pdf

1.4.3 Mesh Topology

Regards,

Mario

0 Kudos
Reply
2,083 Views
zigbee1
Contributor III

Of course I know that documentation, but at any place they are documenting a Controler/Router Sibling relation - where there is no parent -, so please tell us how we should handle such relation in a Mesh network ?

0 Kudos
Reply
2,065 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

 

Hi @zigbee1,

It depends on your Zigbee network, which is the feature of the mesh. The devices, in this case, routers and the coordinator, if they found out a direct connection, they will be neighbour and that is part of the stack.

Also, with the command that you are using you can move on the index value and you will get all the neighbour table for that device.

Regards,

Mario

0 Kudos
Reply
2,112 Views
zigbee1
Contributor III

Any update , thanks ?

0 Kudos
Reply