Hello,
I’d like to adopt KW01Z series for AMI (Advanced Metering Infrastructure) application.
Our MAC standard is 802.15.4e, so I looked over your document EUF-IND-T0970 by Cyril Zarader of BD Microcontrollers EMEA – “Enabling the Internet of Things(IoT)
However I have some questions as below for evaluation
1. How I can get the S/W stack for below layer?
When I installed KW01 Connectivity Software in Website, but I couldn’t find any s/w stack except PHY.
And I need 6TOP s/w stack also in order to drive TSCH, however I couldn’t check it.
2. KW01Z is too small flash memory size for our application, so I’d like to use additional NXP MCU.
It means I only use RF block of KW01Z and s/w stack will be loaded to additional MCU.
If I use additional MCU + KW01Z, can I get the S/W stack?
3. What is PPDU max size of KW01Z?
4. Are transceiver clock(32MHz) and MCU clock(48MHz) clocks needed to input differently?
or can I use one external clock?
Thanks.