Hi anyone.
I am looking for a hardware plattform (RF-TRx or Sytem on chip) for a bigger project, which can be act as an bluetooth (low energy) node -- and on the other hand can be configured to handle a simple proprietary protocoll (without all the BT features), its for compatibility mode.
both configurations are independent, so the are two different firmwares.
best regards / nice weekend
已解决! 转到解答。
The upcoming Kinetis KW41Z will feature (alongside the Bluetooth LE v4.2 capabilities) a generic FSK mode on top of which any proprietary protocol using FSK modulation in the 2.4 GHz band will be implementable.
The upcoming Kinetis KW41Z will feature (alongside the Bluetooth LE v4.2 capabilities) a generic FSK mode on top of which any proprietary protocol using FSK modulation in the 2.4 GHz band will be implementable.
Thank you -- i pick this information for our hardware selection document.
is there a approx. price for the product available ( @ 1kuint) ?
.. or may there are some distributer having this SoC already inside linecard.