Hi anyone.
I am looking for a hardware plattform (RF-TRx or Sytem on chip) for a bigger project, which can be act as an bluetooth (low energy) node -- and on the other hand can be configured to handle a simple proprietary protocoll (without all the BT features), its for compatibility mode.
both configurations are independent, so the are two different firmwares.
best regards / nice weekend
解決済! 解決策の投稿を見る。
The upcoming Kinetis KW41Z will feature (alongside the Bluetooth LE v4.2 capabilities) a generic FSK mode on top of which any proprietary protocol using FSK modulation in the 2.4 GHz band will be implementable.
The upcoming Kinetis KW41Z will feature (alongside the Bluetooth LE v4.2 capabilities) a generic FSK mode on top of which any proprietary protocol using FSK modulation in the 2.4 GHz band will be implementable.
Thank you very much, its what i am looking for.
When the device will be available /released ?
The target is early Q3 2016.
There are however alpha programs you can be part of for early access to the technology. Please contact NXP support for more information.
Thank you -- i pick this information for our hardware selection document.
is there a approx. price for the product available ( @ 1kuint) ?
.. or may there are some distributer having this SoC already inside linecard.