Setting TX power to max values on JN516x devices

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Setting TX power to max values on JN516x devices

1,915 Views
alpay
Contributor I

I have JN5168-001-M05 module (max 9.5dBm) on my gateway and jn5169 SoC (max 10 dBm) on custom end device. How can I set the max tx power levels on these devices?

From the datasheets I have tried,

for JN5168-001-M05 module,

vAppApiSetHighPowerMode(APP_API_MODULE_HPM05, TRUE);
eAppApiPlmeSet(PHY_PIB_ATTR_TX_POWER, (uint32)9);

for JN5169 SoC ,

vAppApiSetHighPowerMode(APP_API_MODULE_STD, TRUE);
eAppApiPlmeSet(PHY_PIB_ATTR_TX_POWER, (uint32)10);

But I did not see any change on distance. What is the exact code for setting the max power level?

Alpay

Tags (2)
3 Replies

1,204 Views
francoisrobbe
NXP Employee
NXP Employee

Hello Alpay,

The usage of eAppApiPlmeSet is described in the JN-UG-3087 (chapter 2.2.1 page 26).

This document can be downloaded from  http://www.nxp.com/products/wireless-connectivity/2.4-ghz-wireless-solutions/ieee-802.15.4-for-jn516...

Best regards

François Robbe

0 Kudos
Reply

1,204 Views
limcb
Contributor IV

On some application note you can see,

/* Define HIGH_POWER_ENABLE to enable high power module */
#ifdef HIGH_POWER_ENABLE
vAHI_HighPowerModuleEnable(TRUE, TRUE);
#endif

Just try TRUE, TRUE.

It looks like no settings to control it to lower power. Only Turn ON High Power and TX at maximum power.

1,204 Views
aonbasi
Contributor II

Thank you Lib.

In JN516x Api datahsheet it is written "This function should only be used with a JN516x high-power module manufactured by NXP." I think it enables external gain circuit assembled on NXP's high power modules. So it can be used for JN5168-001-M05 module but not on NXP's standard JN5169 modules or custom boards that has only JN5169 IC's.

 

The power issues are not clear for JN516x devices.

Alpay

0 Kudos
Reply