The AP gateway ip is 192.168.1.1
One client set static ip 192.168.1.1, then connect to AP
The client will be connected(get 192.168.1.1 due to static ip setting),
but it will make other clients can not access WebUI(http://192.168.1.1)
How to avoid that user using static IP assignment and set the IP to gateway ip(192.168.1.1)?
Is there any uaputl command to disconnect the specific client?
Thanks
You can assign a different IP address as a static address. Usually, the first three ... The address 192.168.1.1 is often pre-assigned to the gateway router.
Hi,
Could you please tell me what part are you using?
Also could you please tell me if you are using a specific SDK example?
Best regards, Daniel.