Hi
Previously, I tried using matter with mw320, but the problem was that there was no BLE, so testing on Homepod mini or SmartThings was not possible.
That is why i conducting tests on RW612.
Q1.
Before testing Matter, I downloaded the SDK, built a sample using mcuxpresso, and debugged it.
I used wifi_cli but it doesn't work properly.
The error below is output.
----------------------------------------------------------------------------------------------------------------------------------
=======================================
wifi cli demo
========================================
MCU wakeup source 0x1...
Initialize CLI
========================================
Initialize WLAN Driver
========================================
4015: [wifi_io] Error: Download firmware failed
4019: [wifi] Error: sd_wifi_init failed. status code -1
4024: [wlcm] Error: wifi_init failed. status code -1
ASSERT ERROR " 0 == result ": file "main.c" Line "321" function name "wlan_driver_init"
----------------------------------------------------------------------------------------------------------------------------------
Also, even if you end debugging and reset the board, nothing is output from the terminal or strange text is displayed.
The current board is written as RD-RW612-BGA IPA-2A/1A V2.
I am attaching a photo to confirm the jumper pin.
I added JLinkDevice.xml and the device to Segger, and programmed the three firmwares (wifi, ble, combo) marked rw610_sb_xxx.bin(SDK/components/conn_fwloader/fw_bin) using J-Link Commander.
Why does this problem occur? Is there any way to solve this?
Q2
I branched a new commit for RW's firmware.
After setting it up by referring to the URL below, activate and "git submodule update --init" worked well, and I even built it using GN and ninja.
https://github.com/NXP/matter/tree/v1.1.0.1-tag-nxp/examples/all-clusters-app/nxp/rt/rw610
Is the gn command below okay?
gn gen out/host --args='chip_enable_matter_cli=true chip_enable_wifi=true chip_enable_ble=true is_debug=true optimize_debug=false chip_with_factory_data=1' ninja -C out/host
And in git it is written as follows:
Does this mean that I need to select the connectedhomeip folder in Existing Code Location?
Or should I select the RW610 folder that was built with ninja?
Thank your support
BR
Bae
Hello,
Thank you in advance for contacting NXP support.
Regarding your questions:
Q1:
Q2:
Also about the pin configuration they are only two changes to be performed on JP42 and JP3 (I attached a image for reference).
Hello
Thank you for your reply.
.> Can you please help me with the board version you are currently using?
It is written V2 on the board.
> Also we suggest to use the latest version of MCUXpresso in this case v11.8.0. (For debug purposes)
Currently using SDK version 2.13.1.
MCUXpresso is also using the latest version.
> Also about the pin configuration they are only two changes to be performed on JP42 and JP3 (I attached a image for reference).
There is no change even if you change the jumper pins.
Thank your support
BR
Bae