Questions about the compatibility between BeeStack and Z-Stack

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Questions about the compatibility between BeeStack and Z-Stack

866 Views
zhaotian
Contributor I

Hi,

Dose anyone know whether the BeeStack of FSL is  compatible with the Z-Stack of IT.They are both based on the provisions by the Zigbee alliance,and if the can work well on the same LAN?

Thanks.

Tags (3)
0 Kudos
Reply
1 Reply

750 Views
AngelC
Senior Contributor I

Dear Zhao,

I am not familiar with the TI’s solution, but both BeeStack and Z-Stack are ZigBee-certified and therefore they have been proven to interoperate properly. Nevertheless, care should be taken to use the same configuration in both vendors’ devices. Parameters such as security keys, network configuration, profile version, etc. are important  to achieve communication between with each other.

If you find any issues when combining both solutions please let us know here so we could give you further recommendations and help you in the process.

Best Regards,

AngelC