Hello,
I operate "qn908xcdk_wireless_examples_bluetooth_private_profile_server_freertos" in MCUXpresso IDE using Development Kit. In the example, after I running the code on IDE, I have to click Button1(SW1) on DK to start wireless BLE communication (after that, the diode D5 turns on RED, and DK try to find private_client).
Here, I want to skip this "press the Button1(SW1)" procedure, and start sending BLE address right away after IDE example is running. How can I do this by modifying the code in "qn908xcdk_wireless_examples_bluetooth_private_profile_server_freertos"?
Thanks,
已解决! 转到解答。
Hello,
Hope you are doing well. The keyboard events are handled by "BleApp_HandleKeys".
If you want to "skip" the usage of the button, you just need to add the "BleApp_Start" function inside the main_task() function, on the line before App_Thread (param);
Hope this helps!
Regards,
Ricardo
Hello,
Hope you are doing well. The keyboard events are handled by "BleApp_HandleKeys".
If you want to "skip" the usage of the button, you just need to add the "BleApp_Start" function inside the main_task() function, on the line before App_Thread (param);
Hope this helps!
Regards,
Ricardo
Thank you for your kind reply.
Your solution works well, and DK starts BLE pairing after the debugging runs without press the button1.
However, it does't stop even after I press the reset button on DK, or terminate the "qn908xcdk_wireless_examples_bluetooth_private_profile_server_freertos" file.
How can I stop the application?
Thanks,