Hello,
This was not the dk board's issue per say. The connectivity Qtool whitelisted the mac address of the dk board and that is why i could not find the dk board on the device panel to connect. By not whitelisting the mac address, I was able to find the dk board with no problem.
Thank you for your suggestion to try the IoT toolbox. I had eliminated that it was not a problem with my board by playing with the IoT toolbox.
Andrew Ha
Hi,
Do you press the button to start the board's advertise?
You can also use our IOT tool box to detect if the board is advertising.
Have a great day,
TIC
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------
Hello,
This was not the dk board's issue per say. The connectivity Qtool whitelisted the mac address of the dk board and that is why i could not find the dk board on the device panel to connect. By not whitelisting the mac address, I was able to find the dk board with no problem.
Thank you for your suggestion to try the IoT toolbox. I had eliminated that it was not a problem with my board by playing with the IoT toolbox.
Andrew Ha