Hello,
I currently have a system with two microcontrollers. One handles BLE and the other handles the signal processing. I am looking for a new microcontroller that can do both.
The QN9080SIP seems to be a good candidate. However, I don't know the signal processing world. I thus have a few questions.
In the software, there are calls to:
- arm_fir_init_f32(): from UM11023 page 214/224, I assume that the FSP is able to execute a FIR up to 16 taps. The code could thus be ported to the FSP.
- arm_sub_f32(), arm_mean_f32(), arm_std_f32(): I have seen nothing in UM11023 that said that the FSP would be able to execute these instructions. These instructions would thus be executed in the Cortex-M4F core.
Am I right ?
Thank you.
Best regards,
Yorick
Hello,
Which software are you checking ? Yes, the Qn9080 will be able to execute those functions due to its core. Maybe this application note will be helpful for you as it explains a little more about the FSP and provides an example application.
Hope it helps.
Regards,
Estephania