Programmable BLE Central Receive Sensitivity

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Programmable BLE Central Receive Sensitivity

跳至解决方案
704 次查看
nidhintomy
Contributor IV

Hi All,

My HW setup is KW45 and SW setup is Central example.

In data sheet of KW45, -97.5 dBm is the receive sensitivity for 1Mbps.
Is it possible for us to change the receive sensitivity? Is there any API. 
If yes, please tell me, which document or api can be used for this purpose?

Best Regards,
Nidhin

标记 (3)
0 项奖励
回复
1 解答
694 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @nidhintomy ,

 

Thanks for contacting NXP support!

KW45's receive sensitivity for 1Mbps is a chip-related indicator, it is not adjustable. It indicates the minimum signal strength that can be correctly received when BER meets the requirements.

 

Hope it helps!

 

Best regards,

Gavin

 

在原帖中查看解决方案

2 回复数
695 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @nidhintomy ,

 

Thanks for contacting NXP support!

KW45's receive sensitivity for 1Mbps is a chip-related indicator, it is not adjustable. It indicates the minimum signal strength that can be correctly received when BER meets the requirements.

 

Hope it helps!

 

Best regards,

Gavin

 

628 次查看
nidhintomy
Contributor IV

Hi @Gavin_Jia ,

Thanks.

0 项奖励
回复