JN5169
AN1219: Dimmer switch, OTA, JN5169, DR1199
Hi, I've got a problem in receiving data through UART1 on JN5169 transmitting from another UART device. It seemed that the "APP_isrUart" is not entered. ( The JN5169 is not in sleeping mode. Probably in doze mode I think since no softtimer is running and no wake event is scheduled.)
The UART TX function is OK, I can get the data which is sent in the UART_vInit funcion from the JN5169.
The initial function involved from APP_vInitialise:
I've tried to send a UART message to JN5169, and to generate a positive pulse when received. But I didn't see that in my oscilloscope.
Hope your help.
Thanks.