I want to know if these products support OS.
If there is an OS available, please let us know which OS types are supported.
Hi @kimhunkt ,
Do you mean OS running on the Host which is connected with PN7462/PN7362 ? If yes, any OS can support. For example, if you make a USB CCID device based on PN7462/PN7362, any OS supporting CCID can work with it.
Hope that makes sense,
Have a great day,
Kan
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------