Hi,
In PN5190B2 datasheet Figure 29. push-pull configuration,RXP connect to TX1 with C R and L,but in SPF-X-PNEV5190B_A1 (page7),RXP connect to TX2 with C and R, so which TX should RXP connect with?
Solved! Go to Solution.
Hello @Fion
This is a symmetrical design, RXN can be connected to TX1 or TX2, and the same goes for RXP. You can refer to the Demo design.
Hello @Fion
This is a symmetrical design, RXN can be connected to TX1 or TX2, and the same goes for RXP. You can refer to the Demo design.
Hi Kelly,
Another question, PN5190B2HN VFLGA40 footprint have 4 thermal pad in the corner, what should i do? connnect with GND or left float? Many thanks.