PCIE8997 fail in WPA3  SEA AP mode ( i.MX8M Plus EVK )

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

PCIE8997 fail in WPA3  SEA AP mode ( i.MX8M Plus EVK )

2,125 Views
changbaoma
Contributor III

Hello, NXP experts

 

My phone act as STA, and i.MX8M Plus EVK board with PCIE8997 act as AP.

My phone can't connect to i.MX8M Plus EVK board with WPA3  SEA  AP mode,but success connect to i.MX8M Plus EVK board with WPA3 SAE transition AP mode. 

And my phone can success connect to other wireless routers with WPA3  SEA  AP mode.

 

I refer to the steps in chapter 2.4.3 WPA3 security of UM11940.pdf to config WPA3  SEA  AP mode.

 

System version info of i.MX8M Plus EVK:

root@imx8mpevk:~# uname -a
Linux imx8mpevk 5.4.70-2.3.2+g5f2220e87dd8 #1 SMP PREEMPT Fri Apr 2 15:53:04 UTC 2021 aarch64 aarch64 aarch64 GNU/Linux

[ 0.000000] Linux version 5.4.70-2.3.2+g5f2220e87dd8 (oe-user@oe-host) (gcc version 9.2.0 (GCC)) #1 SMP PREEMPT Fri Apr 2

[ 0.000000] Machine model: NXP i.MX8MPlus EVK board

 

Is there any things missing in chapter 2.4.3 WPA3 security of UM11940.pdf ?

Can someone check it for me?

 

0 Kudos
7 Replies

2,104 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me with more information of the document you are using ? I do not seem to locate the document you are using as a base.

If the document is under NDA , please send me the link through a message direct here so I can try to duplicate the issue on my side.

 

Regards,
Estephania

0 Kudos

2,069 Views
changbaoma
Contributor III

Hello, @estephania_mart 

Sorry for my delay because of my holidays.

I think you can reproduce WPA3  SEA AP mode connect fail on imx8m plus EVK board when following chapter 2.4.3 WPA3 security of UM11940.pdf

 

0 Kudos

2,051 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me confirm you are using the latest release available in this link for your device ?

 

Regards,

Estephania

0 Kudos

2,045 Views
changbaoma
Contributor III
0 Kudos

2,028 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello,

 

Could you please help me sharing the logs and your configuration file ?

 

Regards,

 

0 Kudos

1,922 Views
changbaoma
Contributor III

Hello,@estephania_mart 

Any suggestion?

0 Kudos

2,022 Views
changbaoma
Contributor III

Hello, @estephania_mart 

Thanks for your continued follow up.

Attached is my logs, included all command and config files.

After doing all steps in my logs, my Phone can found PCIE8997 WPA3 SEA AP (named NXP_Demo), but i can't successfully connect to this AP with error "Denied access to network. connection failed". see below:

changbaoma_0-1644474964433.png

But my phone can successfully connect to other wireless routers with WPA3  SEA  AP mode setuped.

 

Tags (1)
0 Kudos