I use 1229
Connect power after power off, the node can not enter the network。
Only when the node is very close to the coordinator can it enter the network again (5m)
Hi,
The JN-AN-1229 is not saving the Zigbee network, so if you restart the device it will start as factory reset.
Regards,
Mario
Hi,
Is it possible that you could share your question in English?
What is the channel that you are working on? I am assuming that you have the JN module, do you have any interference arround?
Regards,
Mario
I use 5168-m03 and 1229.I tested it indoors without any interference.
I use the router to collect and upload data, and the data transmission is normal in work, but the transmission distance is too close (10 meters), I can't find out the reason, please help me to see what the problem is.