can i know why do you separate NCF3320 and NCJ3320 with temperature range?
Data sheet contents of NCJ3320 cannot be found in NCF3320. Are the functions not available in NCF3320?
NCJ3320 product sheet
8.7.2.21 T4RloadHi register
~
8.7.2.23 T4CounterValHi register
Receiver configuration
8.17.3 RxSynchValH register
~
8.17.5 RxSynchMod register
Hello,
As the device you are using is under NDA and as it is used for automotive applications you will need to go with your DBM (Distributor Business Manager) for further support on this matter as we do not have access to the information. Sorry for the inconvenience may cause.
Have a nice day.
-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!
- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-----------------------------------------------------------------------------