Modify Android-System 4.04 so Wifi-USB would work (Android Car-Radio)

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Modify Android-System 4.04 so Wifi-USB would work (Android Car-Radio)

1,789 次查看
Wolle64
Contributor I
Hello everyone,

I bought a used Android car radio. Kenwood DNN9230. 
Unfortunately the previous owner no longer has the WiFi USB adapter.
Kenwood wrote to me that the adapter is no longer available.
But it should be an adapter with RTL 8188CU. I bought one of these.
Unfortunately it is not recognized on the car radio.

Kenwood support believes that the original adapter has a fixed MAC address. I downloaded the latest update as a zip file for the car radio.
There I can see the entire folder structure and files.

Every time I start, a menu pops up asking me whether I want to log in as an administrator or as a guest.
As an administrator you can only work with an existing WiFi connection.
Even if I had a Wifi connection the request wouldn't work because according to Kenwood the "route-collector" service no longer exists.
My wish is that this query doesn't even appear. Unfortunately you cannot switch this off in the system. My idea now is to adapt the necessary files and then install the update. Would that be possible and if so, what information do you need?
Sorry for my bad english. I used the google-translator and hope it ist good enough. Hope for your help. best regards Wolfgang
0 项奖励
回复
9 回复数

1,761 次查看
Wolle64
Contributor I

Thanks cdoumenc,

No, sorry. Look below there is a screenshot from the content of the updatefile. So, i hope that i could edit some of the files to make run another Wifi-USB. I read about this that the wpa_supplicant, netd, file is needed. But when the original adapter use a fix Mac-adress, i think then a diffrent WIFI-Adapter don`t work, when it use another Mac-adress. Maybe it is possible to change the Mac-adress in the updatefile or to find out in which file are the mac-adress from the Wifi-Adapter. I don`t know.

regards

 

0 项奖励
回复

1,750 次查看
cdoumenc
NXP Employee
NXP Employee

Check in directories "vendor", "wifi" and in PndrBrandingImg.png to get some brand names and know which company you can ask support to.

0 项奖励
回复

1,733 次查看
Wolle64
Contributor I

Thanks for help,

This files are in Wifi and Vendor. In Wifi is a file Wlan.ko. When i open this file there are many files in it. See below. The PndrBrandingImg.png shows only KENWOOD

best regards

 

Wolle64

0 项奖励
回复

1,724 次查看
cdoumenc
NXP Employee
NXP Employee

"I downloaded the latest update as a zip file for the car radio. "
Could you provide the URL where you got this zip if it is public, please ? Or via private message if it isn't.
So that I can check the wifi chipset reference.

In Vendor-lib-kw.JPG, I see "tcc88xx" for which internet searching shows it is a Telechips - Wikipedia
Application Processor based on ARM Cortex-A8 core.

0 项奖励
回复

1,716 次查看
Wolle64
Contributor I

Hi cdoumenc,

 

you are great,

 

here are the link from Kenwood for the latest Update 1.8

https://www.kenwood.com/cs/ce/mm/firmware/2013/2013c/software/DNN_Ver1.8.0.zip

 

best regards

 

Wolle64

0 项奖励
回复

1,608 次查看
cdoumenc
NXP Employee
NXP Employee

In this zip file, I see 2 binaries :

 

PS C:\Users\...\DNN_Ver1.8.0> dir


Directory: C:\Users\...\DNN_Ver1.8.0


Mode LastWriteTime Length Name
---- ------------- ------ ----
-a---l 08/03/2019 14:34 156 programinfo.bin
-a---- 08/03/2019 13:45 506296726 update.kw

 

with an hex editor (http://www.wxhexeditor.org), I don't see anything in programinfo.bin, but, in update.kw, I see, in ASCII/text that wifi linux module name is : system/wifi/wlan.ko

So, I think it is not a NXP wifi chipset since our driver module names are mlan.ko or moal.ko.
So, I suggest that you ask Telechips for support : Telechips

0 项奖励
回复

1,604 次查看
Wolle64
Contributor I

thank you very much.

i could open wlan.ko with 7zip. The content of these files are in my pictures wlan.ko and wlan-2.ko in my post bevor.

i found file .rodata.str1.4 and in there are this: (sorry for many text now)

%s RTKTHREAD ###> rtw_cmd_thread break.................
%s: leaving... check & free all cmd_obj resources
%s: leaving... drop cmdcode:%u
%s: leaving... call up terminate_cmdthread_sema
==> %s , enqueue CMD
rx bc/mc packets, to perform sw rtw_tkip_decrypt
rx bc/mc packets, to perform sw rtw_aes_decrypt
The rx cnt of channel %3d = %d
best_channel_5G = %d
best_channel_24G = %d
_malloc_cnt=%d
_malloc_size=%d
rssi:%d
rxpwdb:%d
signal_strength:%u
signal_qual:%u
noise:%u
free_xmitbuf_cnt=%d, free_xmitframe_cnt=%d, free_ext_xmitbuf_cnt=%d, free_recvframe_cnt=%d
rx_urb_pending_cn=%d
bSurpriseRemoved=%d, bDriverStopped=%d
cur_ch=%d, cur_bw=%d, cur_ch_offet=%d
ht_option=%d
qos_option=%d
pmlmeinfo->state=0x%x
auth_alg=0x%x, enc_alg=0x%x, auth_type=0x%x, enc_type=0x%x
fwstate=0x%x
%s
v3.4.2_3727.20120404 sta_dz_bitmap=0x%x, tim_bitmap=0x%x
sta's macaddr:%02x:%02x:%02x:%02x:%02x:%02x
rtsen=%d, cts2slef=%d
qos_en=%d, ht_en=%d, init_rate=%d
state=0x%x, aid=%d, macid=%d, raid=%d
bwmode=%d, ch_offset=%d, sgi=%d
ampdu_enable = %d
agg_enable_bitmap=%x, candidate_tid_bitmap=%x
sleepq_len=%d
capability=0x%x
flags=0x%x
wpa_psk=0x%x
wpa2_group_cipher=0x%x
wpa2_pairwise_cipher=0x%x
qos_info=0x%x
dot118021XPrivacy=0x%x
tid=%d, indicate_seq=%d
argument size is less than 1
%x invalid set_rssi_disp parameter!
Turn On Rx RSSI Display Function
Turn Off Rx RSSI Display Function
%u %u set %s %u
DBG_SIGNAL_STRENGTH set %s
HW_SIGNAL_STRENGTH argument size is less than 2
%x %x invalid read_reg parameter!
SSID=%s
cur_channel=%d, cur_bwmode=%d, cur_ch_offset=%d
can't get sta's macaddr, cur_network's macaddr:%02x:%02x:%02x:%02x:%02x:%02x
rtw_read8(0x%x)=0x%x
rtw_read16(0x%x)=0x%x
rtw_read32(0x%x)=0x%x
error read length=%d
argument size is less than 3
%x %x %x invalid write_reg parameter!
error write length=%d US EU JP %s unknown country_code:%s
Set SSID under fw_state=0x%08x
Set BSSID under fw_state=0x%08x
%s ID:%u, LEN:%u
%s ID:0x%04x, LEN:%u
MAC Address from efuse error, assign default one !!!
rtw_macaddr_cfg MAC Address = %02x:%02x:%02x:%02x:%02x:%02x
IEEE 802.11 element parse failed (id=%d elen=%d left=%lu)
short vendor specific information element ignored (len=%lu)
short WME information element ignored (len=%lu)
unknown WME information element ignored (subtype=%d len=%lu)
Unknown Microsoft information element ignored (type=%d len=%lu)
Unknown Broadcom information element ignored (type=%d len=%lu)
unknown vendor specific information element ignored (vendor OUI %02x:%02x:%02x len=%lu)
IEEE 802.11 element parse ignored unknown element (id=%d elen=%d)
rtw_issue_addbareq_cmd, p=%d
+rtw_update_ht_cap()
%s(): WLAN_HT_CAP_SM_PS_STATIC
%s IEEE80211_HT_CAP_MAX_AMSDU is set
....AutoSuspend pwrctrlpriv.wepkeymask(%x)
==> rtw_set_key algorithm(%x),keyid(%x),key_mask(%x)
%s
%s, fw_state=%x
roaming from %s(%02x:%02x:%02x:%02x:%02x:%02x), length:%d
roaming do_join return %d
%s(%d) -to roaming fail, indicate_disconnect
%s try another roaming
%s roaming do_join return %d
%s We've try roaming but fail
desired_encmode: %d, privacy: %d
%s: return _FAIL(candidate == NULL)
%s: candidate: %s(%02x:%02x:%02x:%02x:%02x:%02x)
%s: _FW_LINKED while ask_for_joinbss!!!
B A #### Opt_Ant_(%s) , cur_Ant(%s)
[by_bssid:%u][assoc_ssid:%s][to_roaming:%u] new candidate: %s(%02x:%02x:%02x:%02x:%02x:%02x) rssi:%d
try_to_join, but select scanning queue fail, to_roaming:%d
channel plan id error
%s(): channel_set[%d].ChannelNum = %d
%s current operation mode=0x%X
%s new operation mode=0x%X changes=%d
%s
update raid entry, bitmap=0x%x, arg=0x%x
station aid %d exceed the max number
[%s] peermac = %.2X %.2X %.2X %.2X %.2X %.2X
[%s] profileinfo_mac = %.2X %.2X %.2X %.2X %.2X %.2X
[%s] Match!
marc: cannot find SSID for survey event
unknown OUI type!
HT: STA %02x:%02x:%02x:%02x:%02x:%02x HT Capabilities Info: 0x%04x
%s STA %02x:%02x:%02x:%02x:%02x:%02x - no greenfield, num of non-gf stations %d
%s STA %02x:%02x:%02x:%02x:%02x:%02x - 20 MHz HT, num of 20MHz HT STAs %d
%s STA %02x:%02x:%02x:%02x:%02x:%02x - no HT, num of non-HT stations %d
r871x_set_stakey_hdl(): enc_algorithm=%d
r871x_set_stakey_hdl():set_stakey failed, mac_id(aid)=%d
Write CAM, mac_addr=%x:%x:%x:%x:%x:%x, cam_entry=%d
r871x_set_stakey_hdl(): sta has been free
============ linked status check ===================
pathA Rx SNRdb:%d, pathB Rx SNRdb:%d
pathA Rx RSSI:%d,pathB Rx RSSI:%d
pathA Rx PWDB:%d
UndecoratedSmoothedPWDB:%d
Rx RSSI:%d
Rx Signal_strength:%d
Rx Signal_qual:%d
DIG PATH-A(0x%02x), PATH-B(0x%02x)
OFDM -Alarm DA2(0x%04x),DA4(0x%04x),DA6(0x%04x),DA8(0x%04x)
CCK -Alarm A5B(0x%02x),A5C(0x%02x)
FalseAlmCnt_all(%d)
=>%s
report_add_sta_event: add STA
report_del_sta_event: delete STA
survey done event(%x)
report_join_res(%d)
%s, alloc xmitframe fail
%s, alloc xmitbuf fail
%s, category=%d, action=%d, status=%d
BA_starting_seqctrl = %d for TID=%d
rx agg disable tid(%d)
tx agg disable tid(%d)
%s to %02x:%02x:%02x:%02x:%02x:%02x
auth expire %02X%02X%02X%02X%02X%02X
asoc check by DELBA/ADDBA! (pstapriv->expire_to=%d s)(psta->expire_to=%d s), [%02x, %d]
asoc expire by DELBA/ADDBA! (%d s)
asoc check by DELBA/ADDBA! (%d s)
asoc expire %02X%02X%02X%02X%02X%02X
set ch/bw before connected
network.SupportedRates[%d]=%02X
%s(): the rate[%d]=%02X is not supported by STA!
bssrate_len = %d
declare supporting RX STBC
include/net/cfg80211.h link_timer_hdl:no beacon while connecting
link_timer_hdl: auth timeout and try again
link_timer_hdl: assoc timeout and try again
clnt auth fail, status: %d
%s, alloc mgnt frame fail
beacon frame too large
send_beacon, fail!
%s, len=%d
%s(): WLAN_HT_CAP_SM_PS_STATIC
CH=%d, BW=%d, offset=%d
issue_beacon, fail!
update_bmc_sta, mask=0x%x, arg=0x%x
add_RATid_bmc_sta error!
start_create_ibss, invalid cap:%x
no beacon to call receive_disconnect()
[%s] In P2P WPS mode, stay in the peer operating channel = %d
[%s] In
Realtek 8192CU 123456 [%s] P2P State is GONEGO ING!
000 dis pad pbc recv_Action_public_decache, seq_ctrl=0x%x, rxseq=0x%x
[%s] Got GO Nego Req Frame
[%s] Restore the previous p2p state to %d
[%s] Got GO Nego Resp Frame
[%s] Skipped GO Nego Resp Frame (p2p_state != P2P_STATE_GONEGO_ING)
[%s] Got GO Nego Confirm Frame
[%s] Got invite request frame!
[%s] peer address %.2X %.2X %.2X %.2X %.2X %.2X
[%s] match_result = %d
[%s] Got invite response frame!
[%s] Status = %d
[%s] Got Provisioning Discovery Request Frame
[%s] Got Provisioning Discovery Response Frame
%s, action=%d
agg_enable for TID=%d
%s(): DELBA: %x(%x)
%s Reason code(%d)
%s, STA:%02x:%02x:%02x:%02x:%02x:%02x
assoc reject, status code: %d
+OnAuth
auth alg=%x, seq=%X
auth rejected due to bad alg [alg=%d, auth_mib=%d] %02X%02X%02X%02X%02X%02X
going to alloc stainfo for sa=%02X%02X%02X%02X%02X%02X
Exceed the upper limit of supported clients...
(1)auth rejected because out of seq [rx_seq=%d, exp_seq=%d]!
(2)auth rejected because out of seq [rx_seq=%d, exp_seq=%d]!
checking for challenging txt...
auth rejected because challenge failure!(1)
auth rejected because challenge failure!
(3)auth rejected because out of seq [rx_seq=%d, exp_seq=%d]!
handle_assoc(reassoc=%d) - too short payload (len=%lu)
STA %02x:%02x:%02x:%02x:%02x:%02x sent invalid association request
Rx a sta assoc-req which supported rate is empty!
STA included WPS IE in (Re)Association Request - assume WPS is used
STA did not include WPA/RSN IE in (Re)Association Request - possible WPS use
selected_registrar is _FALSE , or AP is not ready to do WPS
STA %02x:%02x:%02x:%02x:%02x:%02x: WPA/RSN IE in association request, but AP don't support WPA/RSN
STA included WPS IE in (Re)Association Request - WPS is used
HT: %02x:%02x:%02x:%02x:%02x:%02x tried to use TKIP with HT association
old AID %d
no room for more AIDs
allocate new AID = (%d)
indicate_sta_join_event to upper layer - hostapd
OnAssocReq OnAssocRsp OnReAssocReq OnReAssocRsp OnProbeReq OnProbeRsp DoReserved OnBeacon OnATIM OnDisassoc OnAuth OnDeAuth OnAction ACTION_SPECTRUM_MGMT ACTION_QOS ACTION_DLS ACTION_BACK ACTION_PUBLIC ACTION_RADIO_MEASUREMENT ACTION_FT ACTION_HT ACTION_SA_QUERY ACTION_WMM ACTION_P2P link to Artheros AP
link to Broadcom AP
link to Marvell AP
link to Ralink AP
link to Cisco AP
link to Realtek 96B
link to Airgo Cap
link to new AP
%s
WMM(%x): %x, %x
%s
Group handshake still in progress !!!
rtw_set_ps_mode(): Busy Traffic , Leave 802.11 power save..
rtw_set_ps_mode(): Enter 802.11 power save mode...
Wait for FW LPS leave too long!!! LPSLeaveTimeOut = %d
==>pwr_state_check_handler .fw_state(%x)
==>ips_leave cnts:%d
==>%s,channel(%d),processing(%x)
==> ips_leave.....LED(0x%08x)...
hw still in rf_off state ...........

%s call autoresume_enter....
======> autoresume fail.............

%s call ips_leave....
======> ips_leave fail.............
%s: bDriverStopped=%d, bup=%d, hw_init_completed=%u
==>ips_enter cnts:%d
==>power_saving_ctrl_wk_hdl change rf to OFF...LED(0x%08x)....

rf_off rf_on @@@@- #1 %s==> rfstate:%s
@@@@- #2 %s==> rfstate:%s
current rf_pwrstate(%s)
==>%s .fw_state(%x)
nRemain_Length is %d and nSubframe_Length is : %d
skb_clone() Fail!!! , nr_subframes = %d
ParseSubframe(): Too many Subframes! Packets dropped!
no buffered packets to xmit
error!psta->sleepq_len=%d
prxattrib->key_index(%d) > WEP_KEYS

recvframe_chkmic:didn't install group key!!!!!!!!!!
mic error :prxattrib->bdecrypted=%d
TX DROP: skb_copy fail!
%s(): skb_is_nonlinear!!
TX DROP: nat25_db_handle fail!
%s()-%d: nat25_db_handle INSERT Warning!
TX DROP: untransformed frame SA:%02X%02X%02X%02X%02X%02X!
TX DROP: skb_linearize fail!
include/linux/netdevice.h <6>netif_stop_queue() cannot be called before register_netdev()
%s(): Enter CTW, change SmartPS
include/net/cfg80211.h RTW_%s:P2P_GO_NEGO_REQ, dialogToken=%d
Rx RTW_%s:P2P_GO_NEGO_RESP, dialogToken=%d
Tx RTW_%s:P2P_GO_NEGO_CONF, dialogToken=%d
RTW_%s:P2P_INVIT_REQ, dialogToken=%d
RTW_%s:P2P_INVIT_RESP, dialogToken=%d
RTW_%s:P2P_DEVDISC_REQ, dialogToken=%d
RTW_%s:P2P_DEVDISC_RESP, dialogToken=%d
RTW_%s:P2P_PROVISION_DISC_REQ, dialogToken=%d
provdisc_req_issued is _TRUE
RTW_%s:P2P_PROVISION_DISC_RESP, dialogToken=%d
RTW_%s:OUI_Subtype=%d, dialogToken=%d
ACTION_CATEGORY_PUBLIC: action=%d, OUI=0x%x, OUI_Subtype=%d, dialogToken=%d
RX TX RTW_%s:P2P_NOTICE_OF_ABSENCE, dialogToken=%d
RTW_%s:P2P_PRESENCE_REQUEST, dialogToken=%d
RTW_%s:P2P_PRESENCE_RESPONSE, dialogToken=%d
RTW_%s:P2P_GO_DISC_REQUEST, dialogToken=%d
%s, action frame category=%d
DIRECT- Realtek DMP Device [%s] p2p_state is %d, ignore!!
[%s] P2P IE not Found!!
[%s] P2P IE Found!!
[%s] Got P2P Capability Attr!!
[%s] Got P2P DEVICE INFO Attr!!
[%s]
[%s] Status = %d
[%s] Ssid = %s, ssidlen = %d
[%s] Peer's operating channel = %d
[%s] WPS IE not Found!!
[%s] GO Intent = %d, tie = %d
[%s] channel count = %d
[%s] channel list attribute not found!
000 dis pad pbc lab [%s] config method = %s
%s
NAT25: malformed IP packet !
NAT25: arp protocol unknown (%4x)!
NAT25: Protocol=Ethernet SNAP %02x%02x%02x%02x%02x
NAT25: Appletalk AARP Sanity check fail!
SID tag length too long!
call skb_pull_and_merge() failed in PADI/R packet!
skb_tailroom() failed in add SID tag!
Discard PPPoE packet due to another PPPoE connection is in progress!
Fail to find PTT_RELAY_SID in FADO!
Invalid PTT_RELAY_SID tag length [%d]!
PADS PADO Can't find MAGIC_CODE in %s packet!
call skb_pull_and_merge() failed in PADO packet!
Discard PPPoE packet due to no connection in progresss!
NAT25: malformed IPv6 packet !
%s %u is large than MAX_XMITBUF_SZ:%u, can't accommodate end cmd
%s %u is large than MAX_XMITBUF_SZ:%u, can't accommodate new cmds
%s rtw_alloc_xmitframe return null
%s rtw_alloc_xmitbuf return null
offset=%x
word_en=%x
data=%x Error, All words disabled
EEPROM ID(%#x) is invalid!!
disable enable BT Coexistance = %s
BlueTooth BT_Ant_Num = Antx2
BlueTooth BT_Ant_Num = Antx1
BlueTooth BT_CoexistType = BT_2Wire
BlueTooth BT_CoexistType = BT_ISSC_3Wire
BlueTooth BT_CoexistType = BT_Accel
BlueTooth BT_CoexistType = BT_CSR_BC4
BlueTooth BT_CoexistType = BT_RTL8756
BlueTooth BT_CoexistType = Unknown
BlueTooth BT_Ant_isolation = %d
BlueTooth BT_Service = BT_OtherAction
BlueTooth BT_Service = BT_SCO
BlueTooth BT_Service = BT_Busy
BlueTooth BT_Service = BT_OtherBusy
BlueTooth BT_Service = BT_Idle
BT_RadioSharedType = 0x%x
Chip Version ID: VERSION_NORMAL_TSMC_CHIP_92C_1T2R.
Chip Version ID: VERSION_NORMAL_TSMC_CHIP_92C.
Chip Version ID: VERSION_NORMAL_TSMC_CHIP_88C.
Chip Version ID: VERSION_NORMAL_UMC_CHIP_92C_1T2R_A_CUT.
Chip Version ID: VERSION_NORMAL_UMC_CHIP_92C_A_CUT.
Chip Version ID: VERSION_NORMAL_UMC_CHIP_88C_A_CUT.
Chip Version ID: VERSION_NORMAL_UMC_CHIP_92C_1T2R_B_CUT.
Chip Version ID: VERSION_NORMAL_UMC_CHIP_92C_B_CUT.
Chip Version ID: VERSION_NORMAL_UMC_CHIP_88C_B_CUT.
Chip Version ID: VERSION_TEST_CHIP_92C.
Chip Version ID: VERSION_TEST_CHIP_88C.
Chip Version ID: VERSION_TEST_UMC_CHIP_8723.
Chip Version ID: VERSION_NORMA_UMC_CHIP_8723_1T1R_A_CUT.
Chip Version ID: VERSION_NORMA_UMC_CHIP_8723_1T1R_B_CUT.
Chip Version ID: ???????????????.
RF_Type is %x!!
Error, bank error, bank=%d
efuseTbl malloc fail !
eFuseWord malloc fail !
eFuseWord[] malloc fail !
=====> rtl8192c_free_hal_data =====
<===== rtl8192c_free_hal_data =====
E-FUSE 93C46 EEPROM type is %s
FirmwareDownload92C():fw reset by itself Fail!!!!!! 0x03 = %x
%s =====> 8051 reset success (%d) .
===> FirmwareDownload91C() fw:Rtl819XFwImageArray_UMC
===> FirmwareDownload91C() fw:Rtl819XFwImageArray_UMC_B
===> FirmwareDownload91C() fw:Rtl819XFwImageArray_TSMC
%s accquire FW from embedded image
Firmware size exceed 0x%X. Check it.
fw_ver=v%d, fw_subver=%d, sig=0x%x
chksum report faill ! REG_MCUFWDL:0x%08x
Polling FW ready fail!! REG_MCUFWDL:0x%08x .
Reset 51 write8 REG_SYS_FUNC_EN:0x%04x
DL Firmware failed!
ConfigFwRelatedForWoWLAN8192CU(): Re-Download Firmware failed!!
ConfigFwRelatedForWoWLAN8192CU(): Re-Download Firmware Success !!
Path A Rx IQK fail!!
Path A IQK Only Tx Success!!
Path A IQK failed!!
Path B Rx IQK fail!!
Path B Only Tx IQK Success!!
Path B IQK failed!!
Path A IQK Success!!
Path B IQK Success!!
IQK:Start!!!
IQK: final_candidate is %x
IQK: RegE94=%x RegE9C=%x RegEA4=%x RegEAC=%x RegEB4=%x RegEBC=%x RegEC4=%x RegECC=%x
Failed Success Path A IQ Calibration %s !
_PHY_PathAFillIQKMatrix only Tx OK
Path B IQ Calibration %s !
===> phy_ConfigBBWithHeaderFile(): do not support test chip
phy_BB8192C_Config_ParaFile():Config to 1T!!
===> phy_ConfigBBWithPgHeaderFile(): do not support test chip
%s(): RF_Save
%s(): RF_Normal
TX_DIR RX_DIR issue_delete_ba : %s...
%s evt_id =0x%x evt_len=0x%x evt_seq=0x%x
%s EVT_EXT_RA_RPT_EID[0x%x] evt_len=0x%x
%s mac_id=%d
%s mac_id=%d psta->init_rate=0x%x
%s evt_id =0x%x evt_len=0x%x
pdmpriv->TxPowerTrackControl = %d
include/net/cfg80211.h Ratio 0x488 =%x
Ratio 0x48c =%x
OFF ON BT_%s
BT set 0x4fd to %x
bRegBT_Sco = %d
Ratio_Tx=%d
Ratio_PRI=%d
bt_sco ==3 Follow Counter
BT TYPE Set to ==> BT_SCO
BT TYPE Set to ==> BT_OtherAction
BT TYPE Set to ==> BT_Busy
BT TYPE Set to ==> BT_PAN
BT TYPE Set to ==> BT_OtherBusy
BT_SCO set 0x4fd to %x
bWifiConnectChange %d, bBtStateChange %d,bRssiStateChange %d
BTCoexit Reg_0x40 (%2x)
BT_Disallow AMPDU
BT_Allow AMPDU RSSI >=40
BT_Allow AMPDU BT Idle
BT_IsolationLow
BT_Turn ON Coexist
BT_Turn OFF Coexist
BT_Turn ON Coexist(Reg0x44 = 0x10100)
BT_Turn OFF Coexist(Reg0x44 = 0x0)
BT in BT_OtherBusy state Tx (%d) >350 parameter(0x%x) = 0x%x
BT in BT_Busy state parameter(0x%x) = 0x%x
BT in BT_SCO state Tx (%d) >160 parameter(0x%x) = 0x%x
BT in BT_SCO state Tx (%d) <160 parameter(0x%x) = 0x%x
BT in State %d and parameter(0x%x) use original setting.
BT set parameter(0x%x) = 0x%x
BT Set RfReg0x1E[7:4] = 0x%x
BT_IsolationHigh
BT_Allow AMPDU bt is off
BT_Turn OFF Coexist bt is off
CheckPbcGPIO - PBC is pressed
BT TYPE Set to ==> BT_Idle
Chip test - check fw write failed, write again..
fw read cmd failed...
IOL %s, polling_ret:0x%02x
error IOL %s complete in %ums
P2P_PS_DISABLE
P2P_PS_ENABLE
P2P_PS_SCAN
P2P_PS_SCAN_DONE
%s(): Mode = %d, SmartPS = %d
==>%s bfwpoll(%x)
beacon frame too large
%s mstatus(%x)
%s
%s(): alloc ReservedPagePacket fail !!!
Set RSVD page location to Fw.
%s() pHalData->fw_ractrl == _TRUE
%s() rtl8192c_set_raid_cmd, bitmap=0x%x, arg =0x%x
usb_write_port_cancel
usb_read_port_cancel
usb_write_port, status=%d
usb_write_port sync, status=%d
###=> urb_write_port_complete status(%d)
bSurpriseRemoved=TRUE
[%s] Buffer len error ,vendor request failed
[%s] pIo_buf == NULL
write read reg 0x%x, usb %s %u fail, status:%d value=0x%x, vendorreq_times:%d
[dvobjpriv:%p][ERROR] continual_urb_error:%d > %d
cannot submit rx in-token(err = 0x%08x),urb_status = %d
###=> usb_read_port_complete => urb status(%d)
ERROR: URB IS IN PROGRESS!/n xmit_tasklet => bDriverStopped or bSurpriseRemoved or bWritePortCancel
recv_tasklet => bDriverStopped or bSurpriseRemoved
recvbuf2recvframe: skb_clone fail
CRC =%x
cant not alloc memory for HAL DATA
==> Disable all dynamic function...
==> Disable DIG...
==> Disable tx power tracking...
==> Turn on all dynamic function...
EEPROMVID = 0x%04x
EEPROMPID = 0x%04x
EEPROMCustomerID : 0x%02x
EEPROMSubCustomerID: 0x%02x
RT_CustomerID: 0x%02x
%s MAC Address from EFUSE = %02x:%02x:%02x:%02x:%02x:%02x
EEPROMRegulatory = 0x%x
_ReadBoardType(%x)
RT_ChannelPlan: 0x%02x
%s...bHWPwrPindetect(%x)-bHWPowerdown(%x) ,bSupportRemoteWakeup(%x)
### PS params=> power_mgnt(%x),usbss_enable(%x) ###
### AntDivCfg(%x)
%s(): REPLACEMENT = %x
====> ReadAdapterInfo8192C
EFUSE EEPROM OK Fail Boot from %s, Autoload %s !
<==== ReadAdapterInfo8192C in %d ms
pwrdown, 0x5c(BIT7)=%02x
GPIO_IN=%02x
print WOWCAM idx =%d
print WOWCAM offset[0] =%x
print WOWCAM offset[1] =%x
print WOWCAM offset[2] =%x
print WOWCAM offset[3] =%x
print WOWCAM offset[4] =%x
update raid entry, mask=0x%x, arg=0x%x
HW_VAR_BASIC_RATE: BrateCfg(%#x)
[HW_VAR_ACM_CTRL] Write 0x%X
==> trigger_gpio_0...
<=== trigger_gpio_0...
Stop RX DMA failed......
%s #####=> 8051 reset failed!.........................
%s =====> 8051 in RAM but !Adapter->bFWReady
SlimComboDbg == TRUE
==> %s
bkeepfwalive(%x)
card disble HWSM...........
card disble without HWSM...........
fw download fail!
fw download ok!
Set RF Chip ID to RF_6052 and RF type to 1T1R.
Set RF Chip ID to RF_6052 and RF type to %d.
==> %s ....
Antenna_A Antenna_B %s,Cur_ant:(%x)%s
BT write 0x%x = 0x%x
BT write 0x%x = 0x%x for non-isolation
BT write 0xC04 = 0x%x
BT write 0xD04 = 0x%x
MAC Address from REG_MACID = %02x:%02x:%02x:%02x:%02x:%02x
%s in %dms
pxmitframe->frame_tag == TXAGG_FRAMETAG
pxmitframe->frame_tag = %d
<4>rx_skb_queue not empty
<4>free_recv_skb_queue not empty, %d
&(&list->lock)->rlock txdmastatu(%x)
==>%s error_status(0x%x)
==> %s wifi_status(0x%x)
%s regc50:0x%08x, regc58:0x%08x, reg824:0x%08x, reg800:0x%08x,
%s REG_TXDMA_STATUS:0x%08x
%s tx hang
%s openFile path:%s fp=%p
%s writeFile, ret:%d
%s openFile path:%s Fail, ret:%d
%s NULL pointer
%s readFile, ret:%d
##########%s########### list poison!!
##########%s###########
##########%s ###########
rtw_wifi &(plock)->rlock pmutex ====> %s...
===> rtw_ips_pwr_down...................
<=== rtw_ips_pwr_down..................... in %dms
===> %s.........
-ips_netdrv_open - drv_open failure, bup=%d
===> rtw_ips_pwr_up..............
<=== rtw_ips_pwr_up.............. in %dms
Can't _rtw_init_xmit_priv
Can't _rtw_init_recv_priv
Can't _rtw_init_sta_priv
register rtw_netdev_ops to netdev_ops
ANY (2)871x_drv - drv_close, bup=%d, hw_init_completed=%d
include/linux/netdevice.h <6>netif_stop_queue() cannot be called before register_netdev()
include/net/cfg80211.h call rtw_indicate_scan_done when drv_close
-871x_drv - drv_close, bup=%d
write_reg read_reg fwstate sec_info mlmext_state qos_option ht_option rf_info ap_info adapter_state trx_info all_sta_info _malloc_cnt best_channel rx_signal rssi_disp ver_info rtl819xC rtl819xD <3>Unable to create rtw_proc directory
Unable to create_proc_read_entry!
Unable to create dir_dev directory
+871x_drv - drv_open, bup=%d
MAC Address = %02x:%02x:%02x:%02x:%02x:%02x
br0 %s()-%d: dev_get_by_name(%s) failed! -871x_drv - drv_open, bup=%d
-871x_drv - drv_open fail, bup=%d
wlan%d +rtw_drv_halt
-rtw_drv_halt
===> rtw_dev_unload
<=== rtw_dev_unload
padapter->bup=%d bDriverStopped=%d bSurpriseRemoved = %d
########### rtw_suspend #################
include/linux/netdevice.h <6>netif_stop_queue() cannot be called before register_netdev()
%s:%d %s(%02x:%02x:%02x:%02x:%02x:%02x), length:%d assoc_ssid.length:%d
########### rtw_suspend done #################
########### rtw_suspend fail !! #################
+rtw_dev_remove
+r871xu_dev_remove, hw_init_completed=%d
usb attached..., try to reset usb device
-r871xu_dev_remove, done
====> autoresume_enter
can't get autopm: %d
...pm_usage_cnt(%d).....
<==== autoresume_enter
rtw driver version=%s
v3.4.2_3727.20120404 Build at: %s %s
May 17 2012 11:44:39 wlan ==>autosuspend_enter...........
########### rtw_resume #################
bkeepfwalive(%x)
enc_algorithm(%x),wepkeymask(%x)
pid[1]:%d
########### rtw_resume done#################
%s, Open net dev failed
########### rtw_resume done with error#################
==> rtw_hw_resume
==> rtw_hw_suspend
%s, failed
CHIP TYPE: RTL8188C_8192C
Detect NULL_CHIP_TYPE

padapter->pwrctrlpriv.bSupportRemoteWakeup~~~~~~

padapter->pwrctrlpriv.bSupportRemoteWakeup~~~[%d]~~~
%s...pm_usage_cnt(%d).....
MAC Address from pnetdev->dev_addr= %02x:%02x:%02x:%02x:%02x:%02x
ui_pid[1]:%d
bDriverStopped:%d, bSurpriseRemoved:%d, bup:%d, hw_init_completed:%d
alloc usb_vendor_req_buf failed... /n
usb_endpoint_descriptor(%d):
bLength=%x
bDescriptorType=%x
bEndpointAddress=%x
wMaxPacketSize=%x
bInterval=%x
RT_usb_endpoint_is_bulk_in = %x
RT_usb_endpoint_is_int_in = %x, Interval = %x
RT_usb_endpoint_is_bulk_out = %x
nr_endpoint=%d, in_num=%d, out_num=%d

USB_SPEED_HIGH
NON USB_SPEED_HIGH
rtl8192cu %s set pid[%d]=%d
%s selector %d error
wpa_set_auth_algs, AUTH_ALG_SHARED_KEY and AUTH_ALG_OPEN_SYSTEM [value:0x%x]
wpa_set_auth_algs, AUTH_ALG_SHARED_KEY [value:0x%x]
wpa_set_auth_algs, AUTH_ALG_OPEN_SYSTEM
wpa_set_auth_algs, AUTH_ALG_LEAP
wpa_set_auth_algs, error!

======= RF REG =======

RF_Path(%x)
0x%02x 0x%08x
0x%05x %s: in=%s
, realmap strcmp OK = %s
rtw_efuse_map_read
OFFSET VALUE(hex)
%s
rtw_efuse_map_read : Fail
0x%02x %s 0x%02x %02X %s %02X %s %s
rmap addr = %x
cnts = %d
(addr + cnts parameter error
rtw_efuse_access error
rtw_efuse_access ok
0x%02x %s 0x%02X %s extra = %s realraw rtw_efuse_access raw ok
%02x %s %02x
%s
mac vidpid ableraw %s : [ available raw size] = %d %s : Command not found
[%s] wps_start = %d
wmap target data = %s
parameter error
rtw_efuse_map_write error
rtw_efuse_map_write ok
wraw cnts = %d
error data for mac addr = %s
Command not found
%s new_ifname:%s
disable%d %s disable
[%s] data = %s

N=%s

N=0000 [%s] extra = %s
wpsCM=

M=%.4d

M=0000 devN= status [%s] Role = %d, Status = %d, peer addr = %.2X:%.2X:%.2X:%.2X:%.2X:%.2X

Status=%.2d
role

Role=%.2d
peer_ifa
MAC %.2X:%.2X:%.2X:%.2X:%.2X:%.2X req_cm

CM=%s
peer_deva
%.2X%.2X%.2X%.2X%.2X%.2X group_id
%.2X:%.2X:%.2X:%.2X:%.2X:%.2X-%s [rtw_wx_set_pmkid] IW_PMKSA_ADD!
[rtw_wx_set_pmkid] BSSID exists in the PMKList.
[rtw_wx_set_pmkid] IW_PMKSA_REMOVE!
[rtw_wx_set_pmkid] IW_PMKSA_FLUSH!
[rtw_wx_set_pmkid] Use the new entry index = %d for this PMKID.
<WIFI@REALTEK> enable= setDN= [%s] %s %d
profilefound= [%s] In value = %s, len = %d
prov_disc= [%s] WiFi Direct is disable!
display keypad pbc label [%s] Unknown WPS config methodn [%s] NOT Found in the Scanning Queue!
nego= [%s] Start PreTx Procedure!
[%s] Not Found in Scanning Queue~
intent= [%s] intent = %d
ssid= [%s] ssid = %s, len = %d
got_wpsinfo= listen_ch= [%s] listen_ch = %d
op_ch= [%s] op_ch = %d
+rtw_wowlan_ctrl: Device didn't support the remote wakeup!!
rtw_wowlan_ctrl: subcode [%d], len[%d], buffer_len[%d]
0x%08x
======= BB REG =======

======= MAC REG =======
871x_driver is only for normal mode, can't enter mp mode
==> trigger gpio 0
==> set dm_bt_coexist:%x
==> delete ba:%x
rtw_read8(0x%x)=0x%02x
rtw_read16(0x%x)=0x%04x
rtw_read32(0x%x)=0x%08x
rtw_write8(0x%x)=0x%02x
rtw_write16(0x%x)=0x%04x
rtw_write32(0x%x)=0x%08x
read_bbreg(0x%x)=0x%x
write_bbreg(0x%x)=0x%x
read RF_reg path(0x%02x),offset(0x%x),value(0x%08x)
write RF_reg path(0x%02x),offset(0x%x),value(0x%08x)
continuous IOL_CMD_WB_REG to 0x%x %u times Success, start:%u, final:%u
continuous IOL_CMD_WB_REG to 0x%x %u times Fail, start:%u, final:%u
continuous IOL_CMD_WW_REG to 0x%x %u times Success, start:%u, final:%u
continuous IOL_CMD_WW_REG to 0x%x %u times Fail, start:%u, final:%u
continuous IOL_CMD_WD_REG to 0x%x %u times Success, start:%u, final:%u
continuous IOL_CMD_WD_REG to 0x%x %u times Fail, start:%u, final:%u
fwstate=0x%x
auth_alg=0x%x, enc_alg=0x%x, auth_type=0x%x, enc_type=0x%x
pmlmeinfo->state=0x%x
qos_option=%d
ht_option=%d
cur_ch=%d
cur_bw=%d
cur_ch_off=%d
sta's macaddr:%02x:%02x:%02x:%02x:%02x:%02x
rtsen=%d, cts2slef=%d
qos_en=%d, ht_en=%d, init_rate=%d
state=0x%x, aid=%d, macid=%d, raid=%d
bwmode=%d, ch_offset=%d, sgi=%d
ampdu_enable = %d
agg_enable_bitmap=%x, candidate_tid_bitmap=%x
tid=%d, indicate_seq=%d
can't get sta's macaddr, cur_network's macaddr:%02x:%02x:%02x:%02x:%02x:%02x
(B)DMFlag=0x%x, arg=0x%x
(A)DMFlag=0x%x
bSurpriseRemoved=%d, bDriverStopped=%d
free_xmitbuf_cnt=%d, free_xmitframe_cnt=%d
rx_urb_pending_cn=%d
sta_dz_bitmap=0x%x, tim_bitmap=0x%x
capability=0x%x
flags=0x%x
wpa_psk=0x%x
wpa2_group_cipher=0x%x
wpa2_pairwise_cipher=0x%x
qos_info=0x%x
dot118021XPrivacy=0x%x
dump rx packet (%d)
###### silent reset test.......#####
==>silent resete cnts:%d
rtw driver version=%s
v3.4.2_3727.20120404 off on turn %s Rx RSSI display function
=== DMFlag(0x%02x) ===
extra_arg = 0 - disable all dynamic func
extra_arg = 1 - disable DIG- BIT(0)
extra_arg = 2 - disable High power - BIT(1)
extra_arg = 3 - disable tx power tracking - BIT(2)
extra_arg = 4 - disable BT coexistence - BIT(3)
extra_arg = 5 - disable antenna diversity - BIT(4)
extra_arg = 6 - enable all dynamic func
wr(0xc50)=0x%x
wr(0xc58)=0x%x
rd(0xc50)=0x%x
rd(0xc58)=0x%x
dbg(0x210)=0x%x
dbg(0x608)=0x%x
dbg(0x280)=0x%x
dbg(0x284)=0x%x
dbg(0x288)=0x%x
dbg(0x664)=0x%x
dbg(0x430)=0x%x
dbg(0x438)=0x%x
dbg(0x440)=0x%x
dbg(0x458)=0x%x
dbg(0x484)=0x%x
dbg(0x488)=0x%x
dbg(0x444)=0x%x
dbg(0x448)=0x%x
dbg(0x44c)=0x%x
dbg(0x450)=0x%x
error dbg cmd!

======== Set channel_plan = 0x%02X ========
+rtw_get_aplist_info
Invalid BSSID '%s'.
BSSID:%02x:%02x:%02x:%02x:%02x:%02x
+rtw_wx_set_enc, flags=0x%x
EncryptionDisabled
rtw_wx_set_enc, key=%d
rtw_wx_set_enc():IW_ENCODE_OPEN
rtw_wx_set_enc():IW_ENCODE_RESTRICTED
rtw_wx_set_enc():erq->flags=0x%x
(keyindex_provided == 1), keyid=%d, key_len=%d
WEP wpa_set_encryption, crypt.alg = WEP
(1)wep_key_idx=%d
wep, set_tx=1
wep, set_tx=0
none TKIP
~~~~stastakey:unicastkey

~~~~stastakey:groupkey
CCMP %s...call rtw_indicate_disconnect

wpa_ie(length:%d):
0x%.2x 0x%.2x 0x%.2x 0x%.2x 0x%.2x 0x%.2x 0x%.2x 0x%.2x
SET WPS_IE
SET WPS_IE, wps_phase==_TRUE
IEEE 802.11bn IEEE 802.11b IEEE 802.11bgn IEEE 802.11bg IEEE 802.11an IEEE 802.11a IEEE 802.11gn IEEE 802.11g unassociated Rates (Mb/s): .5 %d%s wx_get_scan, mcs_rate_bitmap=0x%x
wpa_ie= %02x rsn_ie= %s strlen(msg):%u > IW_CUSTOM_MAX:%u
%s %s
Unknown WPA supplicant request: %d
rtw_add_sta(aid=%d)=%02x:%02x:%02x:%02x:%02x:%02x
rtw_del_sta=%02x:%02x:%02x:%02x:%02x:%02x
rtw_del_sta(), sta has already been removed or never been added
%s, len=%d
rtw_set_encryption(), sta has already been removed or never been added
clear default encryption keys, keyid=%d
r871x_set_encryption, crypt.alg = WEP
r871x_set_encryption, wep_key_idx=%d, len=%d
r871x_set_encryption: pwep allocate fail !!!
%s, set group_key, WEP
%s, set group_key, TKIP
%s, set group_key, CCMP
%s, set group_key, none
%s, set pairwise key, WEP
%s, set pairwise key, TKIP
%s, set pairwise key, CCMP
%s, set pairwise key, none
rtw_get_sta_wpaie, sta_addr: %02x:%02x:%02x:%02x:%02x:%02x
sta's wpa_ie is NONE
%s()-%d: rtw_malloc() ERROR!
Unknown hostapd request: %d
hw still in rf_off state ...........

%s call autoresume_enter....
======> autoresume fail.............

%s call ips_leave....
======> ips_leave fail.............
lps= ips= %u IPS_LEVEL_2 IPS_NORMAL =>%s
ssid=%s, len=%d
<=%s, ret %d
bDriverStopped=%d
IW_SCAN_THIS_ESSID, ssid=%s, len=%d
rtw_wx_set_scan, req->scan_type == IW_SCAN_TYPE_PASSIVE
START STOP %s rssi %d OK LINKSPEED %d MACADDR = %02x:%02x:%02x:%02x:%02x:%02x %*s %s US EU JP CN %s unknown country_code:%s, set to RT_CHANNEL_DOMAIN_FCC
%s rtw_wx_set_channel_plan error
set_mode = IW_MODE_AUTO
set_mode = IW_MODE_ADHOC
set_mode = IW_MODE_MASTER
set_mode = IW_MODE_INFRA
%s()-%d: rtw_xmit() return error!
%s-%d: skb_copy() failed!
pxmitbuf->pxmit_urb[i]==NULL +rtw_indicate_sta_disassoc_event
+rtw_indicate_sta_assoc_event
ASSOCINFO(ReqIEs= %02x ) include/net/cfg80211.h %s
%s, ucast=%d, cipher=0x%x
Unsupported cipher: 0x%x
%s, error rf_type=%d
%s:rf_type=%d
include/net/cfg80211.h remove monitor interface
Couldn't allocate wireless device
Couldn't allocate wiphy device
Couldn't register wiphy device

%s
%s...call rtw_indicate_disconnect

=>%s
privacy=%d, key=%p, key_len=%d, key_idx=%d
%s wdev_priv.block is set
ssid=%s, len=%d
bssid=%02x:%02x:%02x:%02x:%02x:%02x
%s, fw_state=0x%x, goto exit
matched by bssid
matched by ssid
connect, matched == _FALSE, goto exit
%s, wpa_version=%d
%s, nl80211_auth_type=%d
%s(): Shared/Auto WEP
wpa_set_encryption: pwep allocate fail !!!
%s, key_mgt=0x%x
Invalid key mgt: 0x%x
%s, ie_len=%d
set wpa_ie(length:%d):
0x%.2x 0x%.2x 0x%.2x 0x%.2x 0x%.2x 0x%.2x 0x%.2x 0x%.2x
got wpa_ie
got wpa2_ie
SET WPS_IE
SET WPS_IE, wps_phase==_TRUE
%s()-%d: rtw_malloc() ERROR!
set ssid:dot11AuthAlgrthm=%d, dot11PrivacyAlgrthm=%d, dot118021XGrpPrivacy=%d
<=%s, ret %d
%s, mac==%p
%s, mismatch bssid=%02x:%02x:%02x:%02x:%02x:%02x
%s, sta_info is null
+%s
%s, fw_state != FW_LINKED|WIFI_AP_STATE
flush all sta, and cam_entry
free sta macaddr =%02x:%02x:%02x:%02x:%02x:%02x
%s, sta's dot8021xalg = 1 and key_installed = _FALSE
free psta=%p, aid=%d
-%s
%s, beacon_head_len=%d, beacon_tail_len=%d
add bcn, wps_ielen=%d
got p2p_ie, len=%d
Enable P2P function for the first time
enter GO Mode, p2p_ielen=%d
%s, Adding key for %pM
cipher=0x%x
key_len=0x%x
seq_len=0x%x
key_index=%d
pairwise=%d
WEP none TKIP CCMP wpa_set_encryption, crypt.alg = WEP
(1)wep_key_idx=%d
wep, set_tx=1
wep, set_tx=0
%s, : Obtain Sta_info fail
%s, : param->u.crypt.set_tx ==1

~~~~stastakey:unicastkey

~~~~stastakey:groupkey
%s, ret=%d
rtw_set_encryption(), sta has already been removed or never been added
clear default encryption keys, keyid=%d
r871x_set_encryption, crypt.alg = WEP
r871x_set_encryption, wep_key_idx=%d, len=%d
r871x_set_encryption: pwep allocate fail !!!
%s, set group_key, WEP
%s, set group_key, TKIP
%s, set group_key, CCMP
%s, set group_key, none
%s, set pairwise key, WEP
%s, set pairwise key, TKIP
%s, set pairwise key, CCMP
%s, set pairwise key, none
error! fw_state=0x%x, iftype=%d
%s call netdev_open
%s, old_iftype=%d, new_iftype=%d
%s, role=%d, p2p_state=%d, pre_p2p_state=%d
%s, ifname=%s, type=%d
%s, monitor interface(%s) has existed
%s, ndev=%p, pmon_ndev=%p, ret=%d
Unsupported interface type
ndev=%p
radiotap len (should be 14): %d
should be eapol packet
frame_ctl=0x%x
%s, ielen=%d
Got P2P Capability Attr, grp_cap=0x%x, is_GO
[%s] In
rtw_cfg80211_inform_bss error
DIRECT- %s, bBusyTraffic == _TRUE
%s, fwstate=0x%x
%s without scan req
%s, scan abort when device remove
%s, unregister monitor interface
%s : fw_state=_FW_UNDER_SURVEY!
waiting for scan_abort time out!
%s, len=%d, ch=%d, ch_type=%d
channel_type_valid=%d
%s, fc == IEEE80211_STYPE_PROBE_RESP
%s, frame_control == 0x%x
%s, ack=%d
%s channel %02u duration %d
%s remain_ch:%u not in channel plan!!!!
pwdev->sme_state=%d
%s call cfg80211_roamed
Macaddr = %02x:%02x:%02x:%02x:%02x:%02x %s rssi %d include/net/cfg80211.h LinkSpeed %d %s: failed to allocate memory
%s: Android private cmd "%s" on %s
Unknown PRIVATE command %s - ignored
OK %s: bytes_written = %d
%s: failed to copy data to user buffer
START STOP SCAN-ACTIVE SCAN-PASSIVE RSSI LINKSPEED RXFILTER-START RXFILTER-STOP RXFILTER-ADD RXFILTER-REMOVE BTCOEXSCAN-START BTCOEXSCAN-STOP BTCOEXMODE SETSUSPENDOPT P2P_DEV_ADDR SETFWPATH SETBAND GETBAND COUNTRY P2P_SET_NOA P2P_GET_NOA P2P_SET_PS SET_AP_WPS_P2P_IE MACADDR BLOCK

There are named the Wifi-typ RTL8188c

 

I try to connect Telechips-Support and hope, they could help me

 

best regards

 

Wolle64

0 项奖励
回复

1,262 次查看
cdoumenc
NXP Employee
NXP Employee

So, maybe you also need to ask Realtek

0 项奖励
回复

1,767 次查看
cdoumenc
NXP Employee
NXP Employee

Hi Wolle64,

Are you using a NXP WIFI chipset ? If yes, could you fill the following fields, please :


Hw configuration & information
 
NXP Product Name :
Module Maker Name (if any) :
Module Name (if any) :
Host :
WiFi interface :
BT Interface :
15.4 interface :
 
 
Sw configuration & information
 
OS   OS name :
         Kernel version if any :
         MCUxpresso SDK version if any :
         Android version / Kernel Version / WIFI/BT HAL version :
FW   FW version :
Driver   Driver version :

 

Regards

0 项奖励
回复