MKW41Z512VHT4

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

MKW41Z512VHT4

521 次查看
gilles_ngningha
Contributor I

Hello i have a question concerning the microcontroller MKW41Z512VHT4.

in fact we perform a cyclic temperature of our sensor  which includes the part MKW41Z512VHT4.in the design.

After the test between (-40° to 95°C) our sensor failed .

can you please explain if there is a special behavior of this microcontroller with the temperature, especilly for the reset function . thank you for your answer.

标记 (2)
0 项奖励
回复
1 回复

444 次查看
Alexandru-Lilia
NXP Employee
NXP Employee

Hello Gilles,

If you take a look at the reference manual[1], you will see that the temperatures you have tested are the extremes in which the chip should function properly. The temperature probably dropped below or raised above the extremes which caused the chip to function abnormally.

[1] https://www.nxp.com/docs/en/reference-manual/MKW41Z512RM.pdf 

Regards,

Lilian

0 项奖励
回复