MKW41Z512VHT4

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MKW41Z512VHT4

472 Views
gilles_ngningha
Contributor I

Hello i have a question concerning the microcontroller MKW41Z512VHT4.

in fact we perform a cyclic temperature of our sensor  which includes the part MKW41Z512VHT4.in the design.

After the test between (-40° to 95°C) our sensor failed .

can you please explain if there is a special behavior of this microcontroller with the temperature, especilly for the reset function . thank you for your answer.

0 Kudos
Reply
1 Reply

395 Views
Alexandru-Lilia
NXP Employee
NXP Employee

Hello Gilles,

If you take a look at the reference manual[1], you will see that the temperatures you have tested are the extremes in which the chip should function properly. The temperature probably dropped below or raised above the extremes which caused the chip to function abnormally.

[1] https://www.nxp.com/docs/en/reference-manual/MKW41Z512RM.pdf 

Regards,

Lilian

0 Kudos
Reply