Hi everyone,
I have questions about running both BLE and GENFSK on same application and same IC, using MWS MCUXPresso SDK lib AND A FRDM-KW41Z dev board. The application works in this manner:
In order to make all stuffs working, I've followed this custom path, because no example is provided in SDK files:
void Radio_XCVRIdle(){ XCVR_TX_DIG->CTRL &= (XCVR_TX_DIG_CTRL_TX_DFT_EN_MASK | XCVR_TX_DIG_CTRL_LFSR_EN_MASK | XCVR_TX_DIG_CTRL_RADIO_DFT_MODE_MASK); XCVR_TSM->CTRL &= XCVR_TSM_CTRL_FORCE_TX_EN_MASK; XCVR_MISC->DTEST_CTRL &= ~XCVR_CTRL_DTEST_CTRL_DTEST_EN_MASK; }
After this function call, the GENFSK is re-initialized at it's default values with 1Mbps datarate and then the Ble Advertising function it's called.
Now, even if this behavior works, there are two main problems:
So my questions are:
Thanks for the help,
Domenico Virgilio
Hello,
This example has not been implemented yet, so there is no guide on how to achieve that.
To develop it I would suggest you use one of the examples available as a base, remove the other protocol and add the necessary for the GFSK, it would seem that you are going on the correct path do develop it.
Something important to notice it's that when using a hybrid example the radio will be multiplexing between Bluetooth LE and GFSK, so they can't use the radio at the same time.
Regards ,
Estephania
Still no news? Please, I really need help, it's a very urgent task.
Thank you.
Hi, any news?