Long-range WiFi+BT module and EVK suggestion for WiFi signal detection purpose

cancel
Showing results for 
Search instead for 
Did you mean: 

Long-range WiFi+BT module and EVK suggestion for WiFi signal detection purpose

150 Views
alireza1990
Contributor I

I would like to get your opinion on our required WiFi and Bluetooth solution for our product.

Our product is based on Jetson Xavier, and running on ubuntu 16.04. We are looking for integrating one of your chipsets into our product, and use it for WiFi and Bluetooth signal detection, i.e. we're only concerned about receiving and monitoring signals not transmission. We want to get and test several of your recommended modules and EVKs to see which one best fits our requirements. Our main requirements are:

1- Support Dual bands 2.4, 5 GHz

2- Detection range is as far as possible, e.g. built-in LNAs and/or BPF in the chipset can be helpful, also any external LNAs suggestion for this purpose will be appreciated

3- The driver and chip interface support monitor mode.

4- Can be integrated into our Jetson Xavier which is based on ubuntu 16.04.  

5- The driver has the ability to be modified to detect 5MHz and 10MHz signal bandwidths. 


Thank you for your time and consideration in reviewing this inquiry. 

0 Kudos
1 Reply

131 Views
bruce_havemeier
Contributor II

Alireza1990..send me a private email and I'll share with you details on the front-end of our IW416-based module and we can see if it will meet your needs.

 

bruce.havemeier@cel.com

 

Regards-Bruce Havemeier

0 Kudos