Hi,
I want to make a keyboard interrupt during a "while" infinite loop on QN9080. If I use "GETCHAR" or "SCANF", program stop until I press something. But I want to have the loop until I press something (anything) on the keyboard to make an interrupt.
Hello,
Are you using Bluetooth Le? Or are you testing just the board drivers?
You can check the available examples for each in the SKD, there is one for a keyboard that might help you as a guide and one for an HID device working with Bluetooth LE.
If you are just getting started with the QN9080, I would recommend you to check first the driver example and after that check the Bluetooth one.
The examples can be downloaded from the MCUXpresso dashboard .
Regards,
Estephania