Hi
I am studying KW41Z control bridge code.
and I understand how the 'control bridge' receives and parses serial data.
but, I can't understand how the 'control bridge' sends and receives data using ZigBee.
What I want to know,
First, how to transfer message. For example, A board is control bridge, B board is end device.(network joined)
If I send "hello world" from host to A board using UART, A board send "hello world" from A to B using ZigBee. and B board send "hello world" from B to host using UART.
Are there any intuitive example code like this?
Second, I'm analyzing 'ZigBee Control Bridge Code'. but I'm beginner about firmware and rtos. I can't understand ZigBee operation. So how should I study? and What should I look?
thanks
解決済! 解決策の投稿を見る。
Hi JunTae Lee,
Just to confirm, did you run the JN-AN-1216 example?
Do you have a sniffer to capture the packets in the air?
First, Should I define and use a cluster ID?(sAfProfileDataReq.u16ClusterId)
and a profile ID either?(sAfProfileDataReq.u16ProfileId)
Using the ZWGUI you could use a custom cluster.
Second, I can't understand how this function works(APP_eApsProfileDataRequest). could you please explain brief?
and onoff cluster and level cluster use 'eZCL_CustomCommandSend' function. why the raw data option does not use this function(eZCL_CustomCommandSend)?
The on-off cluster has defined the commands and the structures by the ZigBee Spec. Please look at the ZigBee Cluster Library.
Finally, I used raw data option using ZGWUI and checked packet receive in child device.
but It was a simple packet receive debug message. I want to see the Message I send.
Are there other end device example?(I'm using extended light end device example) if not, what should I do?
I recommend using a sniffer for a better debug purpose. Do you have a KW41 dongle?
Regards,
Mario
Hi Mario.
Thanks for the useful answer.
I took a look at ZigBee 3.0 Stack.
and looking at the General options in the ZGWUI, the raw data option.
I have a few questions.
the raw data option
case (E_SL_MSG_SEND_RAW_APS_DATA_PACKET):
{
ZPS_tsAfProfileDataReq sAfProfileDataReq;
uint8 u8DataLength;
sAfProfileDataReq.uDstAddr.u16Addr = ZNC_RTN_U16 ( au8LinkRxBuffer, 1 );
sAfProfileDataReq.u16ClusterId = ZNC_RTN_U16 ( au8LinkRxBuffer, 5 );
sAfProfileDataReq.u16ProfileId = ZNC_RTN_U16 ( au8LinkRxBuffer, 7 );
sAfProfileDataReq.eDstAddrMode = au8LinkRxBuffer[0];
sAfProfileDataReq.u8SrcEp = au8LinkRxBuffer[3];
sAfProfileDataReq.u8DstEp = au8LinkRxBuffer[4];
sAfProfileDataReq.eSecurityMode = au8LinkRxBuffer[9];
sAfProfileDataReq.u8Radius = au8LinkRxBuffer[10];
u8DataLength = au8LinkRxBuffer[11];
u8Status = APP_eApsProfileDataRequest ( &sAfProfileDataReq,
&au8LinkRxBuffer[12],
u8DataLength,
&u8SeqNum );
}
break;
First, Should I define and use a cluster ID?(sAfProfileDataReq.u16ClusterId)
and a profile ID either?(sAfProfileDataReq.u16ProfileId)
Second, I can't understand how this function works(APP_eApsProfileDataRequest). could you please explain brief?
and onoff cluster and level cluster use 'eZCL_CustomCommandSend' function. why the raw data option does not use this function(eZCL_CustomCommandSend)?
Finally, I used raw data option using ZGWUI and checked packet receive in child device.
but It was a simple packet receive debug message. I want to see the Message I send.
Are there other end device example?(I'm using extended light end device example) if not, what should I do?
Thank you again.
and have a nice day.
Hi JunTae Lee,
Just to confirm, did you run the JN-AN-1216 example?
Do you have a sniffer to capture the packets in the air?
First, Should I define and use a cluster ID?(sAfProfileDataReq.u16ClusterId)
and a profile ID either?(sAfProfileDataReq.u16ProfileId)
Using the ZWGUI you could use a custom cluster.
Second, I can't understand how this function works(APP_eApsProfileDataRequest). could you please explain brief?
and onoff cluster and level cluster use 'eZCL_CustomCommandSend' function. why the raw data option does not use this function(eZCL_CustomCommandSend)?
The on-off cluster has defined the commands and the structures by the ZigBee Spec. Please look at the ZigBee Cluster Library.
Finally, I used raw data option using ZGWUI and checked packet receive in child device.
but It was a simple packet receive debug message. I want to see the Message I send.
Are there other end device example?(I'm using extended light end device example) if not, what should I do?
I recommend using a sniffer for a better debug purpose. Do you have a KW41 dongle?
Regards,
Mario
Hi JunTae Lee,
I hope you are doing great.
Sending the hello world like this will not works, the Zigbee protocol works as endpoints and clusters. I recommend to look at the ZigBee 3.0 Stack User Guide Part I: Concept and Operational Information.
If you want to send the hello world like this, you have to create or send this data using a custom cluster.
Look at the General options in the ZGWUI, the raw data option.
Regards,
Mario