KW38 debug by PE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
283件の閲覧回数
LISI1
Contributor I

HI,

 ide:MCUXpresso IDE v11.9.1_2170

I would like to ask a question. At present, when using KW38 chip to develop ble project, we have encountered problems of burning and debugging. Errors are as follows

 

LISI1_0-1718073767530.png

 

LISI1_1-1718073767813.png

 

LISI1_2-1718073767542.png

 

 

Looking forward to your reply, thank you.

0 件の賞賛
返信
1 解決策
266件の閲覧回数
Itzel_UV
NXP Employee
NXP Employee

Hello,

I will be helping you in this case,

 

I notice that you have 3 questions with the topic involving the KW38, by any chance are they related? I that case we can give a follow up on this threat KW38 debug via PEmicro - NXP Community.

 

Regards,

Itzel

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
225件の閲覧回数
LISI1
Contributor I

It's a problem with our board,thank you

0 件の賞賛
返信
267件の閲覧回数
Itzel_UV
NXP Employee
NXP Employee

Hello,

I will be helping you in this case,

 

I notice that you have 3 questions with the topic involving the KW38, by any chance are they related? I that case we can give a follow up on this threat KW38 debug via PEmicro - NXP Community.

 

Regards,

Itzel

0 件の賞賛
返信