when I chose lowpower mode 4, suppose the mcu should be in in VLLS0/1 mode. but it doesn't work.
codes:
已解决! 转到解答。
Hi,
If you are interested in using Low Power features with BLE examples, I would recommend checking the "frdmkw36_wireless_examples_bluetooth_temp_sens_freertos". This example
For more information about this example, you could refer to section "Low Power Temperature Sensor and Collector" from the Bluetooth Low Energy Demo Applications User Guide.pdf (SDK\docs\wireless\Bluetooth)
Hope this helps.
Regards,
Ricardo
Hi
I just tried on my board with the project:frdmkw36_demo_apps_power_mode_switch, the current can reach to 1μA .
But when I try to use frdmkw36_wireless_examples_bluetooth_ancs_c_freertos the current reach to 400μA even though there is only BLE host task and BOARD_BootClockRUN. I don't initialize any pin. How can I fix this? I just want to make the current same as frdmkw36_demo_apps_power_mode_switch runs, about 1μA.
Hi,
If you are interested in using Low Power features with BLE examples, I would recommend checking the "frdmkw36_wireless_examples_bluetooth_temp_sens_freertos". This example
For more information about this example, you could refer to section "Low Power Temperature Sensor and Collector" from the Bluetooth Low Energy Demo Applications User Guide.pdf (SDK\docs\wireless\Bluetooth)
Hope this helps.
Regards,
Ricardo