JN5189 wakeup

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

JN5189 wakeup

731 Views
Viki
Contributor II

Hi All,

The chip I use is JN5189, the SDK version I use is SDK2.6.2_JN5189DK6, and the routine I use is Zigbee_ed_rx_off.
The default setting of this routine can realize the timing wake-up of the device. In addition, I hope to realize that when the module is sleeping, press the wake-up button to immediately wake up the device, and when the wake-up button is released, the module will continue to sleep in accordance with the sleep cycle.
How to realize this function?

BR,

Viki

0 Kudos
Reply
1 Reply

710 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @Viki,

I hope you are doing great.

I recommend looking at the JN-AN-1246 that could help you with the implementation of the button and also the routines that the code implements.

Regards,

Mario

0 Kudos
Reply