I have been experimenting with the JN-AN-1189 Zigbee HA project. Specifically the Dimmer Switch setup. I have set it to performing sampling multiple times per second and sleep when not sampling as I intend to use this on a battery. I am currently having it only TX/RX when necessary but during that roughly 2 second window when it handles the network handshaking I am seeing the unit pull about 13mA of power. Most of this seems to be because the receiver is coming on and staying on during this window (I'm monitoring this via oscilloscope on DIO2). It only transmits in very short bursts(also monitored via oscilloscope on DIO3). The battery I would like to use is not going to support having the receiver on for the entire networking task window even if I can cut it down to 1 second. Is there anything I can do through the JenNet IP stack to limit the time the receiver is on? So far the only option I can find is to switch over to the IEEE 802.15.4 stack which would allow me to shut off the receiver.
Hi Robert,
Could you let us know the following:
Best Regards,
Mario
Mario,
I am using JN-SW-4168, Build version 1279 (per the documentation JN-RN-0058-JN-SW-4168-ZB-HA-ZLL-SDK.pdf)
The application note code is JN-AN-1189-ZigBee-HA-Demo-1v10.
Regards,
Robert
Hi Robert,
This is an issue with the version 1279. This issue was fixed for version 1364 and onwards.
Please use the latest SDK on the website as there has been several issues rectified highlighted in the release notes of the SDK.
The issue was, the receiver is left on while waiting for the association response even though the device will poll for the response.
Best Regards,
Mario
Mario,
Thank you for your response. It looks like I am two revs behind on the SDK and the application note versions so I will update those and run my tests again. I am also on rev behind on the green power and JenOS user guides I was consulting so I will update those as well. Is there an email list I can sign up for that would notify me when releases are made?
Regards,
Robert
Hi Robert,
You can modify your subscription center in your NXP profile.
Please log in and select the option subscription center in the Profile and History.
Then you can select the options that you want and you will receive NXP email updates for products, training, and technical information.In this case you are interesting Interface & Connectivity.
Let me know if you have problems.
Best Regards,
Mario