Hi Chirag,
At 2440 MHz the complex impedance of the JN5169 is 6-j25 in RX mode and 3-j23 in TX mode. An external matching network is needed to transform the impedance to 50 ohm. Since the RX and TX impedance are very close to each other we can achieve a return loss better than -10 dB in both modes.
Best Regards,
Mario
Hi Mario,
Thanks for the support.
It will be really helpful to us.