Dear Sirs,
I have a customized JN5169 board with SKY66111-11 as the front end module.
I am planning to build the firmware of JN-AN-1218 for my JN5169 board.
Where should I set the configurations for PA/LNA (CTX/CRX/CSD/CPS/CHL) in JN-AN-1218?
Thanks!
Solved! Go to Solution.
Hi Alan,
You could add this in the APP_vInitialiseNode, also be sure that set up the correct device that you are working on.
Regards,
Mario
Hi Alan,
Please look at the datasheet and see how the is a block diagram for our modules.
https://www.nxp.com/docs/en/data-sheet/JN5169-001-M0X-2.pdf 7. Block diagram
Please look at the file attached, the set up will depend on the configuration that you have, for example, you could set the power depending on the connections that you have.
Regards,
Mario
Hi Mario,
In order to build the firmware of JN-AN-1218 for my JN5169 board, where can I put the settings in source code? (which .c/.h file?)
Thanks!
Hi Alan,
You could add this in the APP_vInitialiseNode, also be sure that set up the correct device that you are working on.
Regards,
Mario