Hi Mario Ignacio Castaneda Lopez :
Hi JiWei Gao,
This is my UART interrupt configuration.
/* Set UART interrupts */
vAHI_UartSetInterrupt(u8Uart,
asUart[u8Uart].bRtsCts, /* ModemStatus */
TRUE, /* RxLineStatus */
TRUE, /* TxFifoEmpty */
TRUE, /* RxData */
E_AHI_UART_FIFO_LEVEL_1);
Could you please try with another value? a Printable character.
vAHI_UartWriteData(E_AHI_UART_0, 0x31);
Let me know your findings.
Best Regards,
Mario
Hi Mario,
I have the same problem as JiWei ,and I added UART0 operations in JN-AN-1189-zigbee-HA-demo
The UART interrupt (APP_myisrUart(uint32 u32Device, uint32 u32ItemBitmap)) never work,and did not print "isrUart".
How to set up to enter the callback function to process the receiving data?
My UART code as below:
PUBLIC void UART_vInit(void)
{
/* Enable UART 0 */
//vAHI_UartEnable(UART);
bAHI_UartEnable(UART, //uint8 u8Uart,
txbuf, //uint8 *pu8TxBufAd,
(uint8)16, //uint16 u16TxBufLen,
rxbuf, //uint8 *pu8RxBufAd,
(uint8)127); //uint16 u16RxBufLen);
vAHI_UartReset(UART, TRUE, TRUE);
vAHI_UartReset(UART, FALSE, FALSE);
/* Set the clock divisor register to give required buad, this has to be done
directly as the normal routines (in ROM) do not support all baud rates */
UART_vSetBaudRate(UART_BAUD_RATE);
//DBG_vPrintf(TRACE_START, "I THINK IS OK \n");
vAHI_UartSetRTSCTS(UART, TRUE);
vAHI_UartSetControl(UART, FALSE, FALSE, E_AHI_UART_WORD_LEN_8, TRUE, FALSE); /* [I SP001222_P1 279] */
vAHI_Uart0RegisterCallback(APP_myisrUart);
vAHI_UartSetInterrupt(UART, TRUE, TRUE, TRUE, TRUE, E_AHI_UART_FIFO_LEVEL_1); // No TX ints!
DBG_vPrintf(UART_STAR, "I THINK IT IS OK2 \n");
}
PUBLIC void APP_myisrUart(uint32 u32Device, uint32 u32ItemBitmap)
{
DBG_vPrintf(UART_STAR, "isrUart\n");
UART_vTxChar('\n');
UART_vTxChar('i');
UART_vTxChar('s');
UART_vTxChar('r');
UART_vTxChar('U');
UART_vTxChar('\n');
UART_vTxChar('\n');
unsigned int irq = ((*((volatile uint32 *)(UART_START_ADR + 0x08))) >> 1) & 0x0007;
// uint8 u8Byte;
if (irq & E_AHI_UART_INT_RXDATA) {
uint8 u8Byte = u8AHI_UartReadData(UART);
DBG_vPrintf(UART_STAR, "RXUart\n");
// /* if(OS_eGetMessageStatus(&APP_msgSerialRx, &u8Byte) == FALSE)
// {
// /* Failed to send the message to queue */
// }*/
}
if (irq & E_AHI_UART_INT_TX) {
//if(OS_eGetMessageStatus(&APP_msgSerialTx, &u8Byte) == TRUE)
// {
// vAHI_UartWriteData(UART, u8Byte);
/* decrement activity counter for dequeued data */
// } else {
/* disable tx interrupt as nothing to send */
// UART_vSetTxInterrupt(FALSE);
// }
}
}
Thanks
Lucas
Hi Lucas,
I have fixed it as follow:
- Edit file irq_JN516x.S, then add APP_isrUart :
PIC_ChannelPriorities:
.byte 0 # pwm1 priority
.byte 0 # pwm2 priority
.byte 15 # system controller priority
.byte 7 # MAC priority
.byte 0 # AES priority
.byte 0 # PHY priority
.byte 5 # uart0 priority
.byte 0 # uart1 priority
PIC_SwVectTable:
.word vUnclaimedInterrupt # 0
.word vUnclaimedInterrupt # 1
.word vUnclaimedInterrupt # 2
.word vUnclaimedInterrupt # 3
.word vUnclaimedInterrupt # 4
.word APP_isrUart # 5
.word vUnclaimedInterrupt # 6
Regards,
Khac Trung.
that's useful,thanks
That works. Thanks.
Hi Lucas,
Did you solve this issue?
Regards,
Mario
Hi JiWei,
/* Enable UART */
vAHI_UartEnable(u8Uart);
/* Reset UART */
vAHI_UartReset(u8Uart, TRUE, TRUE);
vAHI_UartReset(u8Uart, FALSE, FALSE);
/* Note we've opened the UART */
asUart[u8Uart].bOpened = TRUE;
/* Allow use of RTS/CTS pins with UART if required */
vAHI_UartSetRTSCTS(u8Uart, asUart[u8Uart].bRtsCts);
/* Set baud rate */
vAHI_UartSetBaudDivisor(u8Uart, u16Divisor);
/* Set control */
vAHI_UartSetControl(u8Uart, bEvenParity, bEnableParity, u8WordLength, bOneStopBit, (asUart[u8Uart].u8RxDisable == 0) ? TRUE : FALSE);
/* Using RTS/CTS flow control ? */
if (asUart[u8Uart].bRtsCts)
{
/* Start with RTS on */
UART_vRts(u8Uart, (asUart[u8Uart].u8RxDisable == 0) ? TRUE : FALSE);
/* Is CTS bit set meaning CTS is off ? */
if (u8AHI_UartReadModemStatus(u8Uart) & 0x10)
{
/* Start with transmit disabled */
asUart[u8Uart].u8TxDisable |= UART_ABLE_UARTIO;
}
}
/* Not JenOS ? */
#if !UART_JENOS
{
/* Register callback for appropriate UART */
if (u8Uart == E_AHI_UART_0) vAHI_Uart0RegisterCallback(UART_vInterrupt);
if (u8Uart == E_AHI_UART_1) vAHI_Uart1RegisterCallback(UART_vInterrupt);
}
#endif
/* Set UART interrupts */
vAHI_UartSetInterrupt(u8Uart,
asUart[u8Uart].bRtsCts, /* ModemStatus */
FALSE, /* RxLineStatus */
TRUE, /* TxFifoEmpty */
TRUE, /* RxData */
E_AHI_UART_FIFO_LEVEL_14);
For a better reference please take a look to the JN-AN-1069
For the debug purpose, please
Enable this in the makefile:
Let me know your findings
Regards,
Mario