Interoperability between KW41Z and KW24D

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Interoperability between KW41Z and KW24D

1,110 Views
norishinozaki
Contributor V

Hello,

I'm working with FRDM-KW41Z and FRDM-K64F+FRDM-CR20A Border Router but KW41Z can't join the network(FRDM-KW24D can join).

Isn't there interoperability between Kinetis Thread Stack 1.1 and 1.0.1?

BR,

Nori Shinozaki

Tags (1)
0 Kudos
Reply
2 Replies

926 Views
alejandra_guzman
NXP Employee
NXP Employee

If both MCU have the same Thread spec software, you shouldn't have a problem with a mixed platform network. I think the issue is the software versions you are using.

The KW41z public Thread release comes with Thread v1.1 spec.

I'm guessing you are using a beta version for the FRDM-K64F+FRDM-CR20A  software that is Thread v1.0 spec. 

We are internal testing a Thread v1.1 spec release that will be ready by mid January. Once we launch this software you will be able to have FRDM-K64 border router with FRDM-KW41 devices

926 Views
norishinozaki
Contributor V

Hello aleguzman,

Thanks again, yes I'm using a beta version for FRDM-K64F+CR20A.

Hope to get a next release soon!

Best regards,

Nori Shinozaki

0 Kudos
Reply