According to the networking process in JN-AN-1229, I did not change it, but the routing device could not enter the network of the coordinator. Can you tell me how to set up the network?
I follow this JN-UG-3113 document.To operate.
5.1 Forming a Network
But when you join the network, it always goes wrong.
AN1184_ZBP_Router/Source/app_router.c:192: APP: No event to process!
../../AN1184_ZBP_Router/Source/app_router.c:299: APP: Network discovery complete
../../AN1184_ZBP_Router/Source/app_router.c:304: APP: Found 1 networks
../../AN1184_ZBP_Router/Source/app_router.c:331: APP: Unscanned channels 00000000
../../AN1184_ZBP_Router/Source/app_router.c:332: APP: Ext PAN ID = 0000000000000008
../../AN1184_ZBP_Router/Source/app_router.c:333: APP: Channel = 22
../../AN1184_ZBP_Router/Source/app_router.c:334: APP: Stack Profile = 2
../../AN1184_ZBP_Router/Source/app_router.c:335: APP: Zigbee Version = 2
../../AN1184_ZBP_Router/Source/app_router.c:336: APP: Permit Joining = 1
../../AN1184_ZBP_Router/Source/app_router.c:337: APP: Router Capacity = 1
../../AN1184_ZBP_Router/Source/app_router.c:338: APP: End Device Capacity = 1
../../AN1184_ZBP_Router/Source/app_router.c:343: APP: u64ApsUseExtendedPanid == 0000000000000000 ; u64ExtPanId == 0000000000000000
../../AN1184_ZBP_Router/Source/app_router.c:350: APP: Trying Joining network
../../AN1184_ZBP_Router/Source/app_router.c:360: APP: Failed to join network reason = 8b
../../AN1184_ZBP_Router/Source/app_router.c:192: APP: No event to process!
../../AN1184_ZBP_Router/Source/app_router.c:192: APP: No event to process!
../../AN1184_ZBP_Router/Source/app_router.c:192: APP: No event to process!
../../AN1184_ZBP_Router/Source/app_router.c:192: APP: No event to process!
../../AN1184_ZBP_Router/Source/app_router.c:192: APP: No event to process!
Currently I am using JN-UG-3113, just to let the route and coordinator network, I have not added other content, I just added ZPS_vAplSecSetInitialSecurityState (ZPS_ZDO_PRECONFIGURED_LINK_KEY,
au8DefaultTCLinkKey,
0x00,
ZPS_APS_GLOBAL_LINK_KEY);
The purpose is to solve the ZPS_APL_APS_E_SECURITY_FAIL error.
But now there is ZPS_APL_ZDP_E_NOT_PERMITTED, this error.
I hope to get a reply as soon as possible
1.1229原版肯定没有问题,我们用的也是基于1229的,注意协调器和路由的秘钥及zpsconfig、makefile配置要一致
2.尝试调整大boardcast table 广播表大小
3.把zpsconfig文件贴上来看看
Hi Xuanpu,
Is it possible that you could enter your questions in English?
Regards,
Mario
I said,
1.AN1229 is right without problem, we use too. Attetion that TCLKEY/makefile should be same between router and Coord
2.Try to large Broadcast Transaction Table Size
3.show you zpsconfig
Hi Xuanpu Gu,
I transferred it after I2c, thank you. But at present I have a problem. When I use the IO trigger to wake up the terminal device, I found that during the normal wake-up process, no matter how the IO port is triggered, only one wake-up interrupt can be triggered. I want to ask if you have encountered it.
“ one wake-up interrupt ”--you mean only system controller priority interrupt is generated?
If so, it is right. No matter whether wakeup timer is triggered or DIO is triggered, interrupt only generated in system controller priority interrupt ISR. You should distinguish them by u32AHI_DioInterruptStatus and u8AHI_WakeTimerFiredStatus.
PS: you mentioned terminal device above, is ZED(Zigbee enddevice), I guess
Hi,
Xuanpu is right. the interrupts must be cleared using the functions indicated.
DIO interrupts may be cleared using u32AHI_DioInterruptStatus() or vAHI_DioWakeStatus()
Please look at the https://www.nxp.com/docs/en/user-guide/JN-UG-3075.pdf
Regards,
Mario
Hi
Thank you for your help, the previous problem has been solved.
But now I have encountered new troubles about sending. I know that the normal transmission data is 80 bytes, but when I want to transfer 256 bytes, I find that the transmitted data sometimes fails or there is no ack, and the data does not arrive. End device.
I am using ZPS_eAplAfUnicastAckDataReq to transfer
The errors that occurred are ZPS_APL_APS_E_NO_ACK and ZPS_APL_APS_E_ILLEGAL_REQUEST
I want to know how to make our transmissions safer and data transfer faster?
Thank you for your help and reply 1039521082@qq.com mario_castaneda
Hi,
The errors that occurred are
ZPS_APL_APS_E_NO_ACK The ack issue is from the other device that you have connected
ZPS_APL_APS_E_ILLEGAL_REQUEST A parameter value was out of range.
Did you look at the https://www.nxp.com/docs/en/user-guide/JN-UG-3113.pdf?
B.1 Fragmented Data Transfers
B.1.1 Enabling/Disabling Fragmentation
Please let me know if it helps.
Regards,
Mario
I2c驱动我们用的是FAE提供的,你可以简单描述下问题,我不一定能帮上
I2c driver I used is supplied by NXP FAE, not made by myself. You can simply describle your problem, I may not handle it.
hI,
I am using the JN-AN-1216 Coordinator.
Are you working on the JN-AN-1229 or the JN-AN-1184?
if you are using the 1184. Did you add the code in the app_router.c?
/* Initialise ZBPro stack */
ZPS_eAplAfInit();
ZPS_vAplSecSetInitialSecurityState(ZPS_ZDO_PRECONFIGURED_LINK_KEY,
au8DefaultTCLinkKey,
0x00,
ZPS_APS_GLOBAL_LINK_KEY);
I ran some test with 1229 and it could join the network successfully.
Regards,
Mario
Hi,
Could you please try changing another source file?
Regards,
Mario