I am using the MAYA-W2 module from u-blox for a WiFi Bluetooth Adapter. Since there is the IW611/IW612 populated, maybe some of you can help me. I can easily bring up WiFi using the mwifiex driver and imx-firmware for IW612 but I am not able to bring up Bluetooth:
root@phyboard-pollux-imx8mp-3:~# hciattach /dev/ttymxc2 any 115200 flow
Setting TTY to N_HCI line discipline
Device setup complete
root@phyboard-pollux-imx8mp-3:~# [ 68.060988] Bluetooth: hci0: command 0x1003 tx timeout
[ 70.076990] Bluetooth: hci0: command 0x1001 tx timeout
[ 72.092997] Bluetooth: hci0: command 0x1009 tx timeout
root@phyboard-pollux-imx8mp-3:~# hciconfig hci0 up
[ 88.316175] Bluetooth: hci0: command 0x1003 tx timeout
[ 90.332097] Bluetooth: hci0: command 0x1001 tx timeout
[ 92.348038] Bluetooth: hci0: command 0x1009 tx timeout
Can't init device hci0: Connection timed out (110)
root@phyboard-pollux-imx8mp-3:~# hcitool dev
Devices:
root@phyboard-pollux-imx8mp-3:~#
Can someone help me? Do you havdthis issue already?
Hi,
I will contact you in the other case.
Regards,
Daniel.