I used the coordinator to send data to the terminal node, which immediately stopped working (the entire node module stopped working).How do you solve this?
The data displayed by the serial port is as follows:
What does all this mean?
Why is the node not working?
How to start over?
Now I have a question, I have a node that doesn't need to sleep or Long wake-up time (1 hour), what do I do?
I think there are two related parts in the 1229 template.
1 PWRM_eScheduleActivity(&sWake, SLEEP_TIME, vWakeCallBack);
Change SLEEP_TIME(5 * 32000 ) to SLEEP_TIME(0 * 32000 )。Wake up the device after 0 seconds。
2 in ZTIMER_vWake(); in function vAHI_TickTimerInterval(16000); Change the parameters to make it larger
Can I use it like this?
Hi,
You could add the timer interrupt.
APP_vInitialiseSleepingEndDevice()
{
.
.
.
/* Initialise other software modules
* HERE
*/
//Timer 0 init
DBG_vPrintf(TRUE, "***TMR_vInit***********************\n");
TMR_vInit();
.
.
}
PUBLIC void TMR_vInit(void)
{
DBG_vPrintf(TRUE, "vAHI_DioSetDirection Start\r\n");
vAHI_DioSetDirection(0, 0x10);
/* Make sure no DIO claimed by timer */
vAHI_TimerDIOControl(E_AHI_TIMER_0, FALSE);
vAHI_TimerEnable(E_AHI_TIMER_0, 8, TRUE, TRUE, FALSE);
vAHI_TimerStartRepeat(E_AHI_TIMER_0, 312,625);//312, 625 );
vAHI_DioSetOutput(0x10,0);
}
PUBLIC void vISR_Timer0()
{
static bool toggle = 0x01;
(void) u8AHI_TimerFired(E_AHI_TIMER_0);
if(toggle)
{
toggle = 0x00;
vAHI_DioSetOutput(0,0x10);
}
else
{
toggle=0X01;
vAHI_DioSetOutput(0x10,0);
}
}
Also, you need to modify the irq_JN516x.S
.byte 11 # timer0 priority
.
.
.extern vISR_Timer0
.
.
.
.word vISR_Timer0 # 11
You will see the toggle pin. I tested by my side it works.
Let me know if you have any issues.
Regards,
Mario
Hi,
I was checking the code and you are missing the PDUM_u16APduInstanceWriteNBO. writes the specified data values into the specified APDU instance.
Please look at the code below.
// allocate memory for APDU buffer with preconfigured "type"
PDUM_thAPduInstance data = PDUM_hAPduAllocateAPduInstance( apduMyData );
if( data == PDUM_INVALID_HANDLE )
{
// problem allocating APDU instance memory
DBG_vPrintf(TRACE_APP, "APP: Unable to allocate APDU memory\n");
}
else
{
// read ADC values
int16 sensorValue = 0x5678;
int16 batteryValue = 0x9ABC;
int16 pwmvalue = 0xDEF0;
// load payload data into APDU
uint16 byteCount = PDUM_u16APduInstanceWriteNBO(
data, // APDU instance handle
0, // APDU position for data
"hhh", // data format string
sensorValue,
batteryValue,
pwmvalue
);
if( byteCount == 0 )
{
// no data was written to the APDU instance
DBG_vPrintf(TRACE_APP, "APP: No data written to APDU\n");
}
else
{
PDUM_teStatus pdumStatus = PDUM_eAPduInstanceSetPayloadSize( data, byteCount );
if( pdumStatus != PDUM_E_OK )
{
DBG_vPrintf(TRACE_APP, "SendData: SetPayloadSize error, Status = %d\n", pdumStatus);
PDUM_eAPduFreeAPduInstance( data );
}
else
Regards,
Mario
Hi,
Just to confirm. The coordinator that you are using is JN-AN-1229. Right?
Is the end device getting the bus error?
The process that I am understanding is, you create a Zigbee Network, 1 Coordinator and 1 end device.
-The coordinator sends some data to the end device and after the end device receives this data, the bus error happen.
Could you please confirm this process?
Regards,
Mario
I'm using 1229
Is the end device getting the bus error? yes
Could you please confirm this process? yes i can confirm.
Bus Errors occur when a end device receives and sends data continuously, not once.
Sometimes end device can send and receive data normally for a period of time (from tens of seconds to minutes)
Hi,
You do not have any problem sending data, the issue is after receive and send data the end device enters in a bus error. Is this correct?
The issue that you are facing is not how to send data.
Is the end device in sleep mode? What is the length of the data that you are sending?
Regards,
Mario