The debug messages coming from Coordinator node!
Here's a screenshot of the debug messages coming from SED node
Follow this question ZigBee SED: Unexpected event in E_NETWORK_JOIN -15 while joining a network
To summarize , the AN-1184 is not setting up the HA or ZLL key. This has to be done by the developer although I suggest they could at least have done it for the pre-built binaries and explicitly mentioned how to add it.
If you are using HA profile add the SED following lines of code to app_start_SED.c or otherwise to app_start.c in PRIVATE void vInitialiseApp(void) function just before /* Initialize application */ .
ZPS_vAplSecSetInitialSecurityState(ZPS_ZDO_PRECONFIGURED_LINK_KEY,
(uint8 *)&s_au8LnkKeyArray,
0x00,
ZPS_APS_GLOBAL_LINK_KEY);
Please note that for HA s_au8LnkKeyArray should be defined as follows
PUBLIC uint8 s_au8LnkKeyArray[16] = {0x5a, 0x69, 0x67, 0x42, 0x65, 0x65, 0x41, 0x6c,
0x6c, 0x69, 0x61, 0x6e, 0x63, 0x65, 0x30, 0x39};
compile your app again and it should join the network properly