Hello Friends, davidashraf , mario_castaneda
I am using JN5168-001-M00 Module
i am reading Document like JN-AN-3113 and 3116.
I have create communication between Sleeping Device to Coordinator with major help of NXP Community.
Thank You so much for your support.
Now i just wanted to understand proper ZPS Configuration Tool.
I want to read profile ID , End Point etc.
My Problem:-
1) I can change End Point Number in ZPS Configuration Tool it also reflects to .zpscfg file.
But i wont't be able to Read it.
whenever i change it get error Like PDUM Error because of that My RF Communication get Stop.
What i want:-
1) just wanted to read End Point ID ,Application ID or its Address of Sleeping Device.
Why i want:-
1) Because i wanted to use 20 End Point. so to recognize which End Device send data to Coordinator.
I hope you understand my Problem.
Thank you for your Time
Hello mario_castaneda,
Yes, Mario
i want to send cluster and end point id.
because i just want to understand which end point sends data to coordinator.
just want to says that i try below code
DBG_vPrintf(TRACE_APP, " Profile :%x\r\n", sStackEvent.uEvent.sApsDataIndEvent.u16ProfileId);
DBG_vPrintf(TRACE_APP, " Cluster :%x\r\n",sStackEvent.uEvent.sApsDataIndEvent.u16ClusterId);
DBG_vPrintf(TRACE_APP, " EndPoint:%x\r\n",sStackEvent.uEvent.sApsDataIndEvent.u8DstEndpoint);
DBG_vPrintf(TRACE_APP, "APP: vCheckStackEvent: ZPS_EVENT_APS_DATA_CONFIRM SED Status %d, Address 0x%04x\n",
sStackEvent.uEvent.sApsDataConfirmEvent.u8Status,sStackEvent.uEvent.sApsDataConfirmEvent.uDstAddr.u16Addr);