How to handle E_ZCL_ERR_ZTRANSMIT_FAIL status return?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to handle E_ZCL_ERR_ZTRANSMIT_FAIL status return?

1,088 Views
baskoevoets
Contributor I

I have an application running on my main processor that talks to the Zigbee firmware running on the ZigBee chip (in this case JN5169).

Whenever I send a command to a device that is offline, I stop when I receive the 0x8702 reply (APS Data Confirm Fail).

However, when I now try to send a new command (to the same or a different device), I receive a status message (0x8000) with error code 0x15 (E_ZCL_ERR_ZTRANSMIT_FAIL).

It now takes several seconds before I can send again.

How should I handle E_ZCL_ERR_ZTRANSMIT_FAIL?

Is there a better solution to handle this issue than to wait until I can send again?

I am using using JN-AN-1223 with JN-SW-4168 v1470

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

650 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi,

This authentication interval must be set on all potential parent nodes via the network parameter APS Security Timeout Period

10.7 Advanced Device Parameters

APS Inter-frame Delay

Number of milliseconds between APS data frames. Following transmission of each data block, the APS starts a timer. If there are more unacknowledged blocks to send in the current transmission window then, after a delay of apsInterframeDelay milliseconds the next block is passed to the NWK data service. Otherwise, the timer is set to apscAckWaitDuration seconds.

http://www.nxp.com/documents/user_manual/JN-UG-3101.pdf?fsrch=1&sr=5&pageNum=1 

Hope it helps.

Mario

0 Kudos
Reply