How to change MTU of QN9021

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to change MTU of QN9021

649 Views
seanwu
Contributor IV

Dear sir,

I want to change MTU of QN9021, but I don't know how to change.
Could you please help me?
I use QN9021 wiht SDK1.4.0, lib is qn9021b2_lib_allroles_v40.lib. IDE is Keil.

Thanks.
BR,
Sean Wu

Labels (1)
  • QN

0 Kudos
1 Reply

643 Views
nxf56274
NXP Employee
NXP Employee

Hi,

You can try to change the attm_cfg.h. There is a macro named ATT_DEFAULT_MTU. If this way doesn't work, the program may can't change the MTU. Qn908x also can't change the mtu. The old code does not support this function. 

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos