I want to call the following function to get the JN5169 up to 10dBm transmitting power:
But it doesn't do much in the real world, so how do you get the JN5169 to 10dBm?
Hi Qigong,
Could you please try with the next 2 API?
vAppApiSetComplianceLimits(0, -10, 81);
vAHI_HighPowerModuleEnable(TRUE, TRUE);
For a better reference look at the IEEE 802.15.4 Stack User Guide v2.6
Regards,
Mario
Hello, I still have some questions about 5168 high power and 1229 after reading 333700。
1 、Can I build a zigbee network using only the coordinator and router?Using a router for data collection?
2、I use only the vAppApiSetHighPowerMode(APP_API_MODULE_HPM06,TRUE) function to start the 1229 high-power module,Both of the coordinator and the router。But the transmission distance is very close, does my high power module start correctly?