How do I use UDP under SMAC on the KW2xD platform?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How do I use UDP under SMAC on the KW2xD platform?

453 Views
georgewicks
Contributor II

Is there a way to use UDP under SMAC on the KW24D platform?  It seems like that there is that ability on the KW41Z pltform, BUT looking through the MKW2xD_ConnSw_1.0.1, it doesn't look like it. I have received vague impressions from Freescale/NXP that I should be able to do this, but I can't quite get this pinned down. 

Tags (4)
0 Kudos
1 Reply

353 Views
gerardo_rodriguez
NXP Employee
NXP Employee

Hello George,

SMAC doesn't support UDP. However, the Thread protocol does. Please refer to chapter 8 Socket Commands 
of the Kinetis Thread Stack Shell Interface User Guide document located in <Conn SW path>\docs\wireless\Thread\ for information on how to open a UDP socket from the shell interface.

Also note that the latest version from the Connectivity Software is v1.0.2

Regards,

Gerardo

0 Kudos