I expected two different boards to have different IDs, but they advertise same MAC Address (seen with Android app BLE Scanner) and I don't find any user configurable variable or #define to modify in provided IAR project code.
Thanks
Hi Rodrigo,
You can use the NVDS Configurator tool to set your own BD Address.
Cheers,
Antonio
OK, I see that, but what If I would like to change it from inside the source code? I am working with IAR project provided with QBlue package. I can see Device Name advertised by BLE device can be modified via # define CFG_LOCAL_NAME, but, what about MAC Address? Let´s suppose it is read from NVDS: I can't found in source code which variable it is read to.... I expected to find some RAM variable that would contain MAC address (read from FLASH) and before it was advertised I would modified it as I wish..
Can you help me with that?
Thank you!