Get two NTAG devices (NT3H2211) to talk to one another

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Get two NTAG devices (NT3H2211) to talk to one another

479 Views
andrew_clifford
Contributor II

Hi, is it posible to use one NTAG chip to power up and talk to another?

A bit of background:

I have two NXP microcontroller evaluation boards setup:

  1. QN9080SIP-DK (contains the QN9080-001-M17, a SIP with built-in NT3H2211 chip)
  2. QN9080 DK (contains the QN9080, with no NFC) with a OM23221 board attached (containing a NT3H2211 NFC chip)

I believe these two boards are now effectively the same. The NFC chip is attached to the I2C interface of the MCU in each case.

What i would like to do, ideally is have one of the board wake up the other using NFC. Ultimately, I would like this to trigger a BLE connection, but one step at a time!

Is it possible for the devices to talk to each other in this way? If so, are there and tips/application notes/examples that might be helpful?

Thanks in advance for any help!

Andrew

0 Kudos
Reply
1 Reply

423 Views
estephania_mart
NXP TechSupport
NXP TechSupport

Hello, 

I believe there is a confusion here, the NTAG I2C it's a passive NFC component, which means that it is not able to wake up another tag, you will need an active device in order to wake up the tag.

I would recommend you to check this webinar in order to fully understand more about this. If you have any other doubt, let me know 

Regards,

Estephania 

0 Kudos
Reply