I am using the OM2NTP5332 evaluation board which has NTA5332 device on it. Using the LPCXpresso LPC11U37H board and NTAG5_I2C_Cockpit_v1.1 software I am able to read the configuration registers. The following are some of the examples:
> Reading configuration register I2C_SLAVE_CONFIG: I2C>> S A8 10 3E P I2C>> S A9 54 00 09 02 P > Reading configuration register EHCONFIG: I2C>> S A8 10 3D P I2C>> S A9 00 00 00 00 P > Reading configuration register EDCONFIG: I2C>> S A8 10 3D P I2C>> S A9 00 00 00 00 P > Writing configuration register EHCONFIG: I2C>> S A8 10 3D P I2C>> S A9 00 00 00 00 P I2C>> S A8 10 3D 01 00 00 00 P > Reading configuration register EHCONFIG: I2C>> S A8 10 3D P I2C>> S A9 01 00 00 00 P |
In first case above, it appears that the command being issued is “A8 10 3E”, and the reply to that is “A9 54 00 09 02”. Reading the document “NTP53x2 – NTAG 5 link – NFC Forum-compliant I2C bridge”, I know that “10 3E” is the block address over I2C for I2C_SLAVE_CONFIG.
I have the following questions:
I see that the READ CONFIG request format, as given in Table 115 in the above document is as follows:
Flags | READ CONFIG | Manuf. Code | UID | Block Address | Number of Blocks | CRC16 |
8 bits | 8 bits | 8 bits | 64 bits (optional) | 8 bits | 8 bits | 16 bits |
The only fields I know how to fill are as follows:
Flags | READ CONFIG | Manuf. Code | UID | Block Address | Number of Blocks | CRC16 |
| 0xC0 | 0x4 |
|
| 0 |
|
Thank you in advance for your answers!
解決済! 解決策の投稿を見る。
I hope you are doing fine, as you say A8 in binary is 1010 1000, in the I2C protocol is mentioned that the 8 bit will indicate if either the frame is a read or a write command.
The last bit in 1010 100[0] indicates write, if the sequence is 1010 100[1] this indicates read. This is why you are watching it change from A8 to A9 depending on the command type in the log.
so the slave address register for ntag 5 om2ntp5332 is A8/9 or the default 0x00
Thank you for using our community to answer your questions, we really appreciate it!
I believe that there might be a confusion with the functionality of the NTAG 5, this device has 2 separate interfaces, NFC and I2C.
What you are watching in the Cockpit are the readings from the I2C interface. And the frame from table 115 is for NFC interface.
In order to use the I2C interface with your MCU, please check section 8.3 from the Datasheet. As mentioned in section 8.3.1, the definition is well explained in UM10204. By following this User Manual, you won't have issues implementing the i2c communication with any MCU.
There is an Application Note that might help you understand the implementation of the I2C although it is an I2C master example from the NTAG 5 side, could it be useful for your project.
There is also a series of tutorials from Mobile Knowledge that could be useful for getting started in the development of a solution using NTAG 5.
I hope this information may have been useful!
Thanks for clearing my confusion between I2C and NFC and for sending the links to other useful information.
However, I am still not clear about my question 1. What is “A8” byte in the above sequence – “A8 10 3E”?
Hoping for a fast reply. Thanks.
Please take a look at Figure 22. of UM11406, where a Log window is shown. A8 changes to A9 because as mentioned earlier, it is a 7-bit I2C address that changes its last bit to 1 or 0 depending on if the instruction sent by I2C is for Read or Write.
Please check UM10204 for the full explanation about this matter.
That's what I am confused about! "A8h" in binary is "1010 1000", which clearly occupies 8 bits. So, what is this number representing in this sequence?
Thanks for your support.
I hope you are doing fine, as you say A8 in binary is 1010 1000, in the I2C protocol is mentioned that the 8 bit will indicate if either the frame is a read or a write command.
The last bit in 1010 100[0] indicates write, if the sequence is 1010 100[1] this indicates read. This is why you are watching it change from A8 to A9 depending on the command type in the log.