FP92 p119.2 FW crash of 88W8997, 88W8987 when bring up WiFi if txpower.bin file included.

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FP92 p119.2 FW crash of 88W8997, 88W8987 when bring up WiFi if txpower.bin file included.

Jump to solution
1,245 Views
yao_feng
Contributor III

HW: i.mx8mm or i.mx8mp, + AW-CM358 (88w8987) or Murata 1YM (88W8997)

SW: SDK 6.6.3
WiFi:
Tried NXP EVK board
i.mx8mm
PCIE8997--16.92.21.p119.2-MM6X16437.p3-GPL-(FP92)
SD8987----16.92.21.p119.2-MM6X16437.p3-GPL-(FP92)
Customer side:
i.mx8mp kernel: 5.x
SD8997 ---- 16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL

Ref version:
Tried 
i.mx8mm 6.1.22
SD8987----16.92.21.p76.5-MM5X16391.p3-GPL-(FP92)
PCIE8997--16.92.21.p84.4-MM5X16391.p3-GPL-(FP92)
No issue on this version.

Steps:
1. Convert conf to txpower bin by (refer to UM11490)
./mlanutl mlan0 hostcmd txpwrlimit_cfg_8987.conf generate_raw
txpower.bin
or
./mlanutl mlan0 hostcmd txpwrlimit_cfg_8997.conf generate_raw
txpower.bin

OK:  without this line: txpwrlimit_cfg=nxp/txpower.bin
NOK(FW crash just after load txpower.bin): add this line txpwrlimit_cfg=nxp/txpower.bin

in /lib/firmware/nxp/wifi_mod_para.conf

and then bring up by
modprobe moal mod_para=nxp/wifi_mod_para.conf

FW crash after dmesg
txpwrlimit_cfg=nxp/txpower.bin

Logs share:

NOK logs:
663_p1192_8987_fail.txt
663_p1192_8997_fail.txt

OK logs:
663_p1192_8987_ok_noPwr.txt
663_p1192_8997_ok_noPwr.txt
6122_i.mx8mm_8987.txt
6122_p844_i.mx8mm_8997_noPwr_ok.txt
6122_p844_i.mx8mm_8997_withPwr_ok.txt

Customer can share their logs if needed.
Please help check if the procedure need to be changed after p119.2 
Thanks.

0 Kudos
Reply
1 Solution
1,055 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yao_feng 

I received our internal team feedback as below:

The reported issue is a regression issue and it is fixed already.

We have verified the changes on our local setup and it is working fine.

The release with the fixes will be available in Q2 (end of June). 

Please help to update this info to our end customer and request them to verify on the Q2 release.

Thanks.

 

Best regards,

Christine.

View solution in original post

Tags (1)
8 Replies
1,199 Views
yao_feng
Contributor III

Add logs.

Customer board: i.mx8mp platform
SW: BSP 5.15.129
WiFi version SD8997 ---- 16.92.21.p119.2-16.92.21.p119.2-MM6X16437.P3-GPL-(FP92)
Module: Murata 1YM

Attached logs.
Logs.zip

0 Kudos
Reply
1,161 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yao_feng 

Thanks for creating case to us.

Yes, I can also reproduced locally, and I am checking internally.

Once have any updates, I will let you know.

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply
1,079 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yao_feng 

We are able to observe FW crash/Kernel panic as below on our local setup:

 

Message from syslogd@imx8mpevk at Wed Sep 20 11:32:59 2023 ...

kernel: Internal error: Oops: 0000000096000007 [#1] PREEMPT SMP

Message from syslogd@imx8mpevk at Wed Sep 20 11:32:59 2023 ...

kernel: Code: 91000f9c 1100077b 6b1b029f 54001a0b (38401743)

[ 244.448042] Timeout cmd id (244.444015) ??? [0xecf], act = 0x0

 

We are checking internally for further debugging the issue. We will update you soon.

 

Best regards,

Christine.

Tags (1)
0 Kudos
Reply
1,056 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @yao_feng 

I received our internal team feedback as below:

The reported issue is a regression issue and it is fixed already.

We have verified the changes on our local setup and it is working fine.

The release with the fixes will be available in Q2 (end of June). 

Please help to update this info to our end customer and request them to verify on the Q2 release.

Thanks.

 

Best regards,

Christine.

Tags (1)
639 Views
NancyHuang
Contributor I

Hi @Christine_Li 

Thanks for your reply.

Could you tell us when the new firmware will be available? 6/28?

 

Nancy

0 Kudos
Reply
627 Views
Christine_Li
NXP TechSupport
NXP TechSupport

Hi, @NancyHuang 

We have standalone release completed and available on the nxp.com with secure sign in.

Can you please check if this link can be accessible to you for the Q2 release?

Below link is for 88W8987:

https://www.nxp.com/webapp/sps/download/license.jsp?colCode=SD.GEN.16.92.21.p119.3-MM6X16437.P21-GPL...

Below link is for 88W8997:

Generic_SD-WLAN-UART-BT-8997-LNX_6_6_23-IMX8-16.92.21.p119.3-16.92.21.p119.3-MM6X16437.P21-GPL

Generic_PCIE-WLAN-UART-BT-8997-LNX_6_6_23-IMX8-16.92.21.p119.3-16.92.21.p119.3-MM6X16437.P21-GPL 

If this is not accessible, then you may need to use Q2 (end of June) release available via i.MX BSP or Github release.

 

Thanks,

Christine.

0 Kudos
Reply
1,213 Views
yao_feng
Contributor III

Add more info.
if set
ps_mode=2
auto_ds=2
Got same result.

0 Kudos
Reply
1,241 Views
yao_feng
Contributor III

cont.

0 Kudos
Reply