Error 0x87 - ZPS_XS_E_NO_FREE_EXTENDED_ADDR

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Error 0x87 - ZPS_XS_E_NO_FREE_EXTENDED_ADDR

1,017 Views
zigbee1
Contributor III

We are currently maintaining a  Zigbee controller out of JN5169.
We are using the JN-SW-4170 SDK.
We have of course a good understanding of JN-AN-1216
Application Note: JN-AN-1216 ZigBee 3.0 IoT Control Bridge,

 

Still facing 0x87 - ZPS_XS_E_NO_FREE_EXTENDED_ADDR. The documentation refer to "extended address table", but in none of the documentation this table is defined!

Here are the various parameter definition

MaxNumberNodes70
ActiveNeighbourTableSize50
RoutingTableSize70
AddressMapTableSize20
MacTableSize70
ChildTableSize5
DeviceTableSize70
ZNC_MAX_TCLK_DEVICES70

 

What is wrong ?

0 Kudos
Reply
3 Replies

1,002 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @zigbee1,

What is happening when you get this error?

The coordinator is not accepting a new device? when you are trying to remove a device?

Regards,

Mario

0 Kudos
Reply

996 Views
zigbee1
Contributor III

nothing is done!, no addition nor removal of devices. I just have somehow a stable network at least it behaves like that and get those asynchronous messages.

Could you please clarify what this table is ""extended address table"" as there is no definition of such table in none of the NXP manual

0 Kudos
Reply

972 Views
mario_castaneda
NXP TechSupport
NXP TechSupport

Hi @zigbee1,

The value that the free extended address depends on the sum of the mac table and the map table.

Please try to increase let me know if you are still facing this error.

Regards,

Mario

0 Kudos
Reply