Does wifi ic 88W8801 can support channel 14 and ad-hoc mode and azure rtos ?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Does wifi ic 88W8801 can support channel 14 and ad-hoc mode and azure rtos ?

772件の閲覧回数
chingchung
Contributor I

Hi, NXP:

      We are looking for a wifi ic which can support Japan market ,  Currently we plan to use NXP RT10XX MCU as host cpu.

Here is the questions:

1. Does 88W8801 can suport   wifi  channle 14 in  Japan ( We know 1-13 should be no any problem )

2. Does 88W8801 can  support  ad-hoc mode ?

3. Does  nxp can  provide 88W8801 driver  for Microsoft azure rtos  ?

BR,

ラベル(3)
0 件の賞賛
4 返答(返信)

741件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @chingchung 

1. Does 88W8801 can suport wifi channle 14 in Japan ( We know 1-13 should be no any problem )
From 8801 datasheet, Table 14: Channel Frequencies Supported
channel 14 is not supported.

weidong_sun_0-1666838068461.png

 

2. Does 88W8801 can support ad-hoc mode ?
No, it doesn't.
But 8801 supports Mobile AP interface, it can be used for Access Point.

weidong_sun_1-1666838120180.png

 

3. Does nxp can provide 88W8801 driver for Microsoft azure rtos ?
No, we only have driver for FreeRTOS on MCU platform.

 

Regards,

weidong

0 件の賞賛

730件の閲覧回数
chingchung
Contributor I

Hi, weidong_sun:

Thanks for the answer.   

I has another question does  8801  wifi-direct  function is equal to  Ad-hoc mode ?

BR.

0 件の賞賛

722件の閲覧回数
weidong_sun
NXP TechSupport
NXP TechSupport

Hello @chingchung ,

 

>>I has another question does  8801  wifi-direct  function is equal to  Ad-hoc mode ?

Ad-hoc is different from wfd(WiFi direct), Ad-hoc is wireless networking. wfd is a point-to-point connection mode.

 

Regards,

weidong

0 件の賞賛

764件の閲覧回数
chingchung
Contributor I

Snap98.jpg

0 件の賞賛