Does the inside of the RXD of TJA1043T have pull-up or pull-down applied?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Does the inside of the RXD of TJA1043T have pull-up or pull-down applied?

510 Views
msjang
Contributor I

If not, can I pull-up with 10KR resistance external?

0 Kudos
Reply
1 Reply

503 Views
reyes
NXP TechSupport
NXP TechSupport

Hi,

 

No, there is no internal pull-up or pull-down inside the RXD pin of the TJA1043T, pin RXD reflects the CAN Receiver value, if this is not happening, then an error is occurring.

Typically, this pin is directly connected to the uC without the need of an external pull-up.

 

If you are asking this because you need smooth the edges at bit transitions, I guess it would be better to use an up to 1 kΩ series resistor of on pin TXD.

 

Regards,

Jose Reyes

0 Kudos
Reply