Does elftosb 5.1.19 support KW38 / KW39 series?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Does elftosb 5.1.19 support KW38 / KW39 series?

跳至解决方案
959 次查看
wenhuafeng
Contributor II

1.JPG

KW38/KW39 are not found in the series supported by elftosb 5.1.19. Which series does the KW38/KW39 BLE chip belong to?

0 项奖励
1 解答
914 次查看
wenhuafeng
Contributor II

Hi TIC,

Secure boot functions such as those described in document AN12283, not FLASH encryption functions.

TKS!

在原帖中查看解决方案

0 项奖励
6 回复数
943 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

KW should belong to kinetis. You can have a try.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
938 次查看
wenhuafeng
Contributor II

Hi TIC,

I asked the technical support of nxp and said that the kw series elftosb does not support it, please help confirm?

thank you very much!

0 项奖励
925 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

Yes. It seems the kw is different from kinetis series. I am not sure if it will be added in the future.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
923 次查看
wenhuafeng
Contributor II

Hi TIC,

Our project requires secure boot. Does the kw38/kw39 series support secure boot? No relevant information can be found on the nxp official website.

Thank you every much!

0 项奖励
917 次查看
nxf56274
NXP Employee
NXP Employee

Hi,

No. If you want to protect your flash from reading or erasing. You can configure 'Flash configuration'.

12.PNG

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 days after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
915 次查看
wenhuafeng
Contributor II

Hi TIC,

Secure boot functions such as those described in document AN12283, not FLASH encryption functions.

TKS!

0 项奖励